iMX6 Quad Sabre AI CPU2 Board do not support Ethernet Port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 Quad Sabre AI CPU2 Board do not support Ethernet Port

618 Views
zhengliangwu
Contributor I

 CPU2.pngCPU1.png1. the ethernet port  is different between iMX6Q Sabre AI CPU and CPU2 Card.

2.

1) Under the same linux kernel of 3.10.17 version,   the Ethernet port on the old board, iMX6Q Sabre AI CPU Card can work well, but not work on the new board, iMX6Q Sabre AI CPU2 Card.

2) Meanswhile, the ehternet port on CPU2 board works well on the 4.19 linux kernel.
3. It's sure that the question of ethernet port comes from the the change of ethernet port hardware.

1) Can the new CPU2 Board still support the old linux kernel 3.10.17???
2) About 1) above, how to change the linxu kernel 3.10.17 to support the ethernet port on CPU2 board???

0 Kudos
2 Replies

506 Views
igorpadykov
NXP Employee
NXP Employee

Hi  Zhengliang

Sabre AI CPU2 Card  is new board and you are right, it is supported

only in latest kernels. For helping with porting its drivers to older kernels one

can apply to Professional Services:

NXP Professional Services|NXP 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

506 Views
zhengliangwu
Contributor I

Boot Log about Ethernet Port:

Configuring network interfaces... fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
udhcpc (v1.22.1) started
Sending discover...
libphy: 2188000.ethernet:01 - Link is Up - 100/Full
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Sending discover...
Sending discover...
No lease, failing

0 Kudos