iMX6: Problem of synchronization IPU with Gstreamer 1.0 YOCTO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6: Problem of synchronization IPU with Gstreamer 1.0 YOCTO

563 Views
gaylordlebrun
Contributor II

Hello to all,


When I want recorded)a video with "imxv4l2src" source element, I notice, during the review or if I show directly my video flow in the screen, the IPU does not reach in synchronized. Which can be the cause of it?

Thank you in advance for quite answer,
Gaylord

PS: examle pipeline: gst-launch-1.0 imxv4l2src device=/dev/video0 ! video/x-raw, width=1920, height=1080 ! overlaysink

Labels (3)
0 Kudos
1 Reply

462 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gaylord

one can try kernel boot parameter dmfc=3  and with lower

resolutions to check if this is caused by performance issues.

Recheck gstreamer usage with sect.7.5 Overlaysink usage atatched

Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

0 Kudos