iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.

1,844件の閲覧回数
feriaxue
Contributor I

Why is this?Who can help me? Thanks a lot

iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.

CLK setup,by OpenEmbed---

CLK setup,by OpenEmbed

IMX PCIe pcie_rst, 0.

IMX PCIe pcie_rst, 1.

PCIE: imx_pcie_pltfm_probe start link up.

link up failed, DB_R0:0x004a4a02, DB_R1:0x08000000!

IMX PCIe port: link down!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,171件の閲覧回数
minshi
Contributor I

Can you tell me, how do you solve this problem?

0 件の賞賛
返信

1,171件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Feria

in general one can follow recommendations given in

IMX PCIe port: link down! with atheros pcie

git.denx.de Git - u-boot.git/commitdiff

or check the Link training sequence with scope and

use http://cache.freescale.com/files/32bit/doc/app_note/AN4784.pdf

for tweaking eye diagram.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信