iMX6 PCB footprint

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 PCB footprint

Jump to solution
1,183 Views
omda
Contributor I

Hi,

I would like to ask if iMX6(Quad/Dual/DuallLite/Solo) have the same PCB footprint and signal assignement? Which means when I design a board based on iMX6, is it possible to used iMX6 Quad or iMX6 Dual or iMX6 Solo with the same PCB footprint?

Omda,

Labels (6)
0 Kudos
Reply
1 Solution
910 Views
igorpadykov
NXP Employee
NXP Employee

Hi Omda

iMX6 Quad and Dual fully interchangable, for Solo one needs to look

carefully at  AN4397 Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite.

Packages one can find in sect.6 Package Information and Contact Assignments

IMX6DQCEC , IMX6SDLCEC  and footprints in

i.MX6_SABRE_AI_DESIGNFILES : Design files, including hardware schematics, layout files

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
911 Views
igorpadykov
NXP Employee
NXP Employee

Hi Omda

iMX6 Quad and Dual fully interchangable, for Solo one needs to look

carefully at  AN4397 Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite.

Packages one can find in sect.6 Package Information and Contact Assignments

IMX6DQCEC , IMX6SDLCEC  and footprints in

i.MX6_SABRE_AI_DESIGNFILES : Design files, including hardware schematics, layout files

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
910 Views
omda
Contributor I

Hi Igor,

Thank you for your reply.

Kind regards.

Omda,

0 Kudos
Reply