iMX6_MAX board is rebooting after flashing QNX sdp7.0 BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6_MAX board is rebooting after flashing QNX sdp7.0 BSP

ソリューションへジャンプ
2,528件の閲覧回数
chethankumar
Contributor III

Hi,

I downloaded QNX BSP from below link

QNX SDP 7.0 for i.MX platforms - Boundary Devices 

I copied bootscript and qnx-ifs to the sd card and put that inside iMX6_MAX board. My board is rebooting again and again. Please find the log below i am seeing during u-boot. Please help me to resolve this issue.

U-Boot 2015.07-15072-g45cfc85 (Jan 28 2016 - 17:41:33 -0700), Build: jenkins-uboot_v2015.07-30

CPU: Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)
Reset cause: WDOG
Board: Nitrogen6_max
I2C: ready
DRAM: 3.8 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
SF: Detected SST25VF016B with page size 256 Bytes, erase size 4 KiB, total 2 MiB
auto-detected panel hannstar7
Display: hdmi:1920x1080M@60 (1920x1080)
In: serial
Out: serial
Err: serial
Net: using phy at 6
FEC [PRIME], usb_ether
Hit any key to stop autoboot: 0
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: ncq stag pm led clo only pmp pio slum part
No port device detected!
** Bad device size - sata 0 **
switch to partitions #0, OK
mmc0 is current device
reading /6x_bootscript
195 bytes read in 11 ms (16.6 KiB/s)
## Executing script at 10008000
reading qnx-ifs
11301012 bytes read in 512 ms (21 MiB/s)
Starting QNX...
## Starting application at 0x10800000 ...

U-Boot 2015.07-15072-g45cfc85 (Jan 28 2016 - 17:41:33 -0700), Build: jenkins-uboot_v2015.07-30

CPU: Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)
Reset cause: WDOG
Board: Nitrogen6_max
I2C: ready
DRAM: 3.8 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
SF: Detected SST25VF016B with page size 256 Bytes, erase size 4 KiB, total 2 MiB
auto-detected panel hannstar7
Display: hdmi:1920x1080M@60 (1920x1080)
In: serial
Out: serial
Err: serial
Net: using phy at 6
FEC [PRIME], usb_ether
Hit any key to stop autoboot: 0
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: ncq stag pm led clo only pmp pio slum part
No port device detected!
** Bad device size - sata 0 **
switch to partitions #0, OK
mmc0 is current device
reading /6x_bootscript
195 bytes read in 11 ms (16.6 KiB/s)
## Executing script at 10008000
reading qnx-ifs
11301012 bytes read in 512 ms (21 MiB/s)
Starting QNX...
## Starting application at 0x10800000 ...

Thanks,

CK@

タグ(2)
1 解決策
2,244件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

Yes, this question was answered via our support channel.

Please try not to cross post your questions.

Regards,

Gary

元の投稿で解決策を見る

3 返答(返信)
2,244件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello gary_bisson, would you know what could be the cause of this behavior?

Regards,

2,245件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

Yes, this question was answered via our support channel.

Please try not to cross post your questions.

Regards,

Gary

2,244件の閲覧回数
chethankumar
Contributor III

Thank you for the reply.

Regards,

CK

0 件の賞賛
返信