iMX6 LVDS0 and HDMI in SOLO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 LVDS0 and HDMI in SOLO

924 Views
tamilarasane
Contributor III

Hi

is iMX6 solo will support HDMI and LVDS0 at a time..?

HDMI and LVDS1 are working at a time in iMX6 solo . But HDMI and LVDS0 is not working.

Thanks,

Tamilarasan

0 Kudos
Reply
2 Replies

666 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tamilarasan

yes i.MX6S hardware support this configuration, please

pay attention to IOMUXC_GPR3 selections and pinmux

configurations

HDMI.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

666 Views
hyobokahn
Contributor II

Hello.

I'm trying to make mirror display on LVDS and HDMI.

But, I fail and I guess my driver do not support dual display(mirror display).

I use kernel and driver from Youcto build.

I try after change UBoot video option and device tree.

but, I think this is not work, only display fb0 device only.

Where is the point to modify IOMUXC_GPR3 setting on Linux driver.

is there any place to get working device driver?

 

Thanks.

0 Kudos
Reply