iMX6 HDMI interlaced formats

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 HDMI interlaced formats

Jump to solution
1,441 Views
mariocasto
Contributor II

Hello to everybody,

For what I do understand for now on the iMX6 HDMI interface is possible only to use progressive resolution.

For a project that I should start I need also 720x576@50i, 720x480@59.94i, 1920x1080@50i, 1920x1080@59.94i.

Is there any roadmap to have these resolutions available on iMX6 HDMI interface?

Regards,

Mario

1 Solution
820 Views
jimmychan
NXP TechSupport
NXP TechSupport

No plan to support interlace mode for HDMI now.

View solution in original post

0 Kudos
3 Replies
821 Views
jimmychan
NXP TechSupport
NXP TechSupport

No plan to support interlace mode for HDMI now.

0 Kudos
820 Views
jayaramks
Contributor III

Hi,

Any update on supporting interlaced format on imx6 HDMI?

Regards,

Jayaram.

820 Views
jayaramks
Contributor III
0 Kudos