iMX6 - GPU2D information

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6 - GPU2D information

2,230 次查看
adrianthewlis
Contributor III

The iMX6DQRM has a bunch of information about what the GPU2D can do, but no register spec. or information of how.

Is there another doc. with more information, or is there any sample code available?

标签 (2)
标记 (1)
0 项奖励
回复
3 回复数

1,839 次查看
gary_bisson
Senior Contributor III

Hi,

You can ask your Freescale or Distributor local FAE for help on getting more information.

Another way to get started on the GPU (2D or 3D), is to look at the fsl-gpu-sdk which provides examples and some documentation about it.

https://www.freescale.com/webapp/Download?colCode=i.MX-GPU-SDK-2-1&appType=license&location=null&fps...

There is a Yocto recipe for it:

meta-fsl-demos/recipes-graphics/fsl-gpu-sdk at master · Freescale/meta-fsl-demos · GitHub

Regards,

Gary

0 项奖励
回复

1,839 次查看
adrianthewlis
Contributor III

Gary, thanks for the response.

I downloaded fsl-gpu-sdk a few days ago, but when I opened the .tgz there was a .bin file with a Linux shell script tacked on the front. My guess is its a form of self-extracting archive. Is there a non-Linux way of accessing this, or is a there a regular archive (eg. zip) of the same contents?

How would I find my FAE? I am based in the San Fran Bay Area. Alternately, the board we are working with is from Toradex, should I go through them?

0 项奖励
回复

1,839 次查看
gary_bisson
Senior Contributor III

Hi Adrian,

You are right this is a self-extracting archive which requires you to agree to the EULA. This is why you won't find just a regular zip file of it. If you want to extract it on Windows, I'd look at Cygwin but you won't be able to build the examples using it.

As for the FAE, yes Toradex should be able to help you getting in touch with the right person.

Regards,

Gary

0 项奖励
回复