iMX6 Dual - Bug PCIe with i210 device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 Dual - Bug PCIe with i210 device

759 Views
micheldasilva
Contributor I

Hi,

I designed a board with an iMX6 Dual processor. On the PCI express, I linked an I210-IT ( Intel Ethernet Controller PCIe v2.1 2.5GT/s).

|------------------|                                               |------------------|

|   iMX6D        |                                              |    I210-IT       |

|            Clk1   | --------------||-------------------->| PCE_Clk      |

|       PCIe TX | ---------------||-------------------->| PCE RX       |

|       PCIe Rx |<--------------||----------------------| PCE TX       |

| -----------------|                                               |------------------|

For the reference Clock PCIE, I used the output CLK1_P/N to synchronize I210 RefClock. Is it correct or wrong?

I used linux issue YOCTO version 4.1.15_1.0.0.

Sometimes, PCIe  bugs to the READ access and more rarely, to the WRITE access. Have you any suggestions about this problem?

Sincerely,

Michel

Labels (1)
0 Kudos
1 Reply

374 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michel

this may be caused by weak signal due to improper layout or noise.

One can try to adjust parameters of PCIe_PHY by changing the IOMUXC_GPR8 register

settings described in AN4784 PCIe Certification Guide for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite

http://www.nxp.com/assets/documents/data/en/application-notes/AN4784.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos