iMX6 DDR3 Calibration Failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 DDR3 Calibration Failure

1,703 Views
SreedharNair
Contributor I

Hi,

I am trying to run DDR3 calibration for imx6 quad processor (MCIMX6Q5EYM10AC) with 4 memory chips (MT41K256M16TW-107) in flyby topology using only CS0. I am running V3.0 of the test script (aid document attached). Please see log below

============================================

        DDR Stress Test (3.0.0)

        Build: Dec 14 2018, 14:12:06

        NXP Semiconductors.

============================================

============================================

        Chip ID

CHIP ID = i.MX6 Dual/Quad (0x63)

Internal Revision = TO1.2

============================================

============================================

        Boot Configuration

SRC_SBMR1(0x020d8004) = 0x00000000

SRC_SBMR2(0x020d801c) = 0x30000001

============================================

ARM Clock set to 1GHz

============================================

        DDR configuration

BOOT_CFG3[5-4]: 0x00, Single DDR channel.

DDR type is DDR3

Data width: 64, bank num: 8

Row size: 15, col size: 10

Chip select CSD0 is used

Density per chip select: 2048MB

============================================

Current Temperature: 43

============================================

DDR Freq: 396 MHz

ddr_mr1=0x00000000

Start write leveling calibration...

running Write level HW calibration

  MPWLHWERR register read out for factory diagnostics:

  MPWLHWERR PHY0 = 0x00003878

HW WL cal status: no suitable delay value found for byte 2

HW WL cal status: no suitable delay value found for byte 3

  MPWLHWERR PHY1 = 0x1e1e1e3c

Write leveling calibration completed but failed, the following results were found:

    MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x0043004E

    MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x001F001F

    MMDC_MPWLDECTRL0 ch1 (0x021b480c) = 0x001D0030

    MMDC_MPWLDECTRL1 ch1 (0x021b4810) = 0x00110015

Write DQS delay result:

   Write DQS0 delay: 78/256 CK

   Write DQS1 delay: 67/256 CK

   Write DQS2 delay: 31/256 CK

   Write DQS3 delay: 31/256 CK

   Write DQS4 delay: 48/256 CK

   Write DQS5 delay: 29/256 CK

   Write DQS6 delay: 21/256 CK

   Write DQS7 delay: 17/256 CK

 

WARNING: write-leveling calibration value is greater than 1/8 CK.

                Per the reference manual, WALAT must be set to 1 in the register MDMISC(0x021B0018).

                This has been performed automatically.

                However, in addition to updating the calibration values in your DDR initialization,

                it is also REQUIRED change the value of MDMISC in their DDR initialization as follows:

    MMDC_MDMISC (0x021b0018) =  0x00011740

Error: failed during write leveling calibration

Please help.

Regards,

Sreedhar

SreedharNair_0-1642346499684.png

 

Labels (2)
0 Kudos
Reply
3 Replies

1,658 Views
disheng
Contributor III

Density per chip select: 2048MB

this does not match with your configuration.

0 Kudos
Reply

1,663 Views
art
NXP Employee
NXP Employee

The most likely cause of the issue is the PCB-level design issue e.g. trace
length mismatch, impedance mismatch etc. Check your PCB design against the
recommendations, given in the Hardware Development Guide for i.MX 6QuadPlus,
6Quad, 6DualPlus, 6Dual, 6DualLite, 6Solo Families of Applications Processors
document, available on the processor's Documentation web page:

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

Best Regards,
Artur

0 Kudos
Reply

1,685 Views
SreedharNair
Contributor I

Any help is high appreciated.  

Regards,

Sreedhar Nair

0 Kudos
Reply