iMX53x community Hw design support - wall comments

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX53x community Hw design support - wall comments

1,287 Views
JCP
Contributor I

Community group to help and share knowledge and information to develop boards based on iMX53x processors

0 Kudos
7 Replies

1,074 Views
JayPark
Contributor I

I have just started my development project with iMX 53.

In order to reduce development time, I am investigating possible development packages, and I have found out some useful development boards from several providers.

My requirements are as follows.

- CPU module add-on board style

- CPU module pin description should be provided

- CPU module should have MII pins

- CPU module should have UART pins

- BSP software source files should be provided.

- PCB schematic files should be provided

If there is someone who has experience of successful start with existing iMX 53 development packages, please recommend me good one.

If you do not want to open your comments in public, please send me a message.

Thank you!

0 Kudos

1,074 Views
iMXAndrew
Contributor II

@Prabu Kumar. Also does the board have Window Embedded Compact 7 Driver and instructions on how to use it?

0 Kudos

1,074 Views
iMXAndrew
Contributor II

@Prabu Kumar. I like the solution. However, my 7" touchscreen (MCIMX51LCD kit) already uses the connector. Is there anyway to hook up the 2 devices to the same connector.

0 Kudos

1,074 Views
PrabuKumar
Contributor I

@Andrew Hurley Check out this daughter card to give composite input to iMX53 QSB kit. http://www.e-consystems.com/NTSC-PAL-Video-Decoder-Board-iMX53x.asp

0 Kudos

1,074 Views
iMXAndrew
Contributor II

Anyone know how I can make a composite video input to either the iMX53 QSB or the iMX53 Sabre Tablet?

0 Kudos

1,074 Views
marshachang
NXP Employee
NXP Employee

The part number is MCIMX-LVDS1. 

0 Kudos

1,074 Views
Vincent_ng
Contributor I

What's the PN of the 10.1” 1024x768 display with capacitive multi-touch for SABRE?

What's the price of Infineon Amazon-1 3G Module (optional) ?

 

Thank you!

0 Kudos