iMX53QSB: DirectFB and TSlib

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX53QSB: DirectFB and TSlib

3,994 Views
gonfer
Contributor V

Hi all,

 

I'm trying to setup DirectFB working with TSlib. Under Ltib, I've selected Dialog DA9052 TSI to support the touch controller, and I can compile without errors.

When the QSB is booting I can see the TSI driver is loaded. This has been extracted from the boot log:

DA9052 TSI Device Driver, v1.0
input: da9052-tsi as /class/input/input0
TSI Drv Successfully Inserted da9052-tsi

These are the exports I'm using:

export TSLIB_CALIBFILE=/etc/pointercal
export TSLIB_CONFFILE=/usr/etc/ts.conf
export TSLIB_TSDEVICE=/dev/input/event0
export TSLIB_PLUGINDIR=/usr/lib/ts
export TSLIB_CONSOLEDEVICE=none

Thanks to the patch that Shlomo Kut posted here http://imxcommunity.org/group/imx53quickstartboard/forum/topics/seiko-wvga-panel-with-imx53?commentI... now I'm able to run ts_calibrate OK, but DirectFB (df_input) doesn't work.

Under /usr/lib/directfb-1.4-5/inputdrivers I can only see libdirectfb_linux_input.so. I think libdirectfb_tslib.so should also be there, but I'm not able to locate this file in my system ¿?.

 

Then, when I run df_input, I get the following:

root@freescale ~$ df_input                             

   ~~~~~~~~~~~~~~~~~~~~~~~~~~| DirectFB 1.4.13 |~~~~~~~~~~~~~~~~~~~~~~~~~~
        (c) 2001-2010  The world wide DirectFB Open Source Community
        (c) 2000-2004  Convergence (integrated media) GmbH
      ----------------------------------------------------------------

(*) DirectFB/Core: Single Application Core. (2011-10-03 09:59)
(*) Direct/Memcpy: Using libc memcpy()
(*) Direct/Thread: Started 'VT Switcher' (-1) [CRITICAL OTHER/OTHER 0/0] <8388608>...
(*) Direct/Thread: Started 'VT Flusher' (-1) [DEFAULT OTHER/OTHER 0/0] <8388608>...
(*) DirectFB/FBDev: Found 'DISP3 BG' (ID 0) with frame buffer at 0x8e000000, 32768k (MMIO 0x00000000, 0k)
(*) Direct/Thread: Started 'Linux Input' (-1) [INPUT OTHER/OTHER 0/0] <8388608>...
(*) DirectFB/Input: mma8450 0.1 (directfb.org)
(*) Direct/Thread: Started 'Hotplug with Linux Input' (-1) [INPUT OTHER/OTHER 0/0] <8388608>...
(*) DirectFB/Input: Hot-plug detection enabled with Linux Input Driver
(*) DirectFB/Graphics: Generic Software Rasterizer 0.6 (directfb.org)
(*) DirectFB/Core/WM: Default 0.3 (directfb.org)
(*) Direct/Interface: Loaded 'FT2' implementation of 'IDirectFBFont'.
(*) FBDev/Mode: Setting 800x480 RGB16
(*) FBDev/Mode: Switched to 800x480 (virtual 800x1440) at 16 bit (RGB16), pitch 1600
(*) Direct/Interface: Loaded 'PNG' implementation of 'IDirectFBImageProvider'.

Exiting PEN DOWN HANDLER
The raw data count is 10
The OS data count is 2
PEN UP DECLARED
Exiting PEN DOWN HANDLER
The raw data count is 10
The OS data count is 2
PEN UP DECLARED

 

In the LCD I'm getting readings from the mma8450, but the touch screen is not working.

The contents of /dev/input/ is:

root@freescale ~$ ls -l /dev/input
crw-r-----    1 root     root      13,  64 Jan  1 04:42 event0
crw-r-----    1 root     root      13,  65 Jan  1 04:42 event1

and the input devices in my system are:

root@freescale ~$ cat /sys/class/input/input0/name
da9052-tsi
root@freescale ~$ cat /sys/class/input/input1/name
mma8450

 

Just to see what happens, I have also exported TSLIB_TSDEVICE as:

export TSLIB_TSDEVICE=/dev/input/event1

In this case ts_calibrate doesn't work (as expected) but, for a while, I can get touch screen events in df_input ¿¿¿???? This is what I see when running df_input:

~~~~~~~~~~~~~~~~~~~~~~~~~~| DirectFB 1.4.13 |~~~~~~~~~~~~~~~~~~~~~~~~~~
        (c) 2001-2010  The world wide DirectFB Open Source Community
        (c) 2000-2004  Convergence (integrated media) GmbH
      ----------------------------------------------------------------

(*) DirectFB/Core: Single Application Core. (2011-10-03 09:59)
(*) Direct/Memcpy: Using libc memcpy()
(*) Direct/Thread: Started 'VT Switcher' (-1) [CRITICAL OTHER/OTHER 0/0] <8388608>...
(*) Direct/Thread: Started 'VT Flusher' (-1) [DEFAULT OTHER/OTHER 0/0] <8388608>...
(*) DirectFB/FBDev: Found 'DISP3 BG' (ID 0) with frame buffer at 0x8e000000, 32768k (MMIO 0x00000000, 0k)
(*) Direct/Thread: Started 'Linux Input' (-1) [INPUT OTHER/OTHER 0/0] <8388608>...
(*) DirectFB/Input: da9052-tsi 0.1 (directfb.org)
(*) Direct/Thread: Started 'Hotplug with Linux Input' (-1) [INPUT OTHER/OTHER 0/0] <8388608>...
(*) DirectFB/Input: Hot-plug detection enabled with Linux Input Driver
(*) DirectFB/Graphics: Generic Software Rasterizer 0.6 (directfb.org)
(*) DirectFB/Core/WM: Default 0.3 (directfb.org)
(*) Direct/Interface: Loaded 'FT2' implementation of 'IDirectFBFont'.
(*) FBDev/Mode: Setting 800x480 RGB16
(*) FBDev/Mode: Switched to 800x480 (virtual 800x1440) at 16 bit (RGB16), pitch 1600
(*) Direct/Interface: Loaded 'PNG' implementation of 'IDirectFBImageProvider'.

 

Something is messed up here. Please, could someone point me what I'm missing?

 

Thanks,

Gonzalo.

 


Labels (1)
6 Replies

2,913 Views
Oceanblue
Contributor III

Hi Gonzalo, have you solved the TSlib issue? we have meet the exact same issue to you, now we can calibrate TP, but it seem the system still can't work it.

      anyone have idea on MX53 QSB touch panel ? thx.

Jack

0 Kudos
Reply

2,913 Views
gonfer
Contributor V

Hi Jack,

no, I didn't investigate this issue more deeply - I switched to a project based on an iMX28 and am not working any longer with the QSB. Have you checked if the problem comes from udev?

Hope someone else can assist you.

Gonzalo.

0 Kudos
Reply

2,913 Views
gonfer
Contributor V

Nope !

I tried different kernels, different DirectFBs and different TSlibs with no luck. I've also found the same problem in the iMX25PDK, so I've ended up managing TSLib by my own, not under DirectFB.

If you finally get the combo working, please, share your experience.

Gonzalo.

0 Kudos
Reply

2,913 Views
SteveSparks
Contributor I

Gonzalo,

I am having the exact same issue. I have engaged Freescale support but no resolution yet. 

Did you have any luck?

 

Thanks,

Steve

0 Kudos
Reply

2,912 Views
gonfer
Contributor V

Thanks Daiane,

I have doublechecked my setup against imxdev.org and looks everything is OK, but doesn't work in the QSB.

I'll follow your advice about DirectFB mailing list.

 

Gonzalo

0 Kudos
Reply

2,912 Views
daiane_angolini
NXP Employee
NXP Employee

You can take a look here:

http://www.imxdev.org/wiki/index.php?title=I.MX31_PDK_Board_DirectFB

I hope it can help you

 

But I would recommend you to look for help on Direct FB maillist.

 

When you got it working, please share the results over here.

0 Kudos
Reply