Hi,
I try to activate the DMA with UART5 on a custom board with the kernel linux-2.6.35, but when I do exchange data on uart, I have a DMA_ERROR sr1:2040 sr2:508a (or sr1=2010 sr2:5089) .
I try to change the size of different received buffers ( UART5_DMA_RXBUFSIZE from serial.h , or RXDMA_BUFF_SIZE from mxc_uart.c ) but nothing change, i always have the same error.
The uart in normal mode at 115200 bauds works well but i need to increase the baud rate up to 2,000,000 .
Is there any solution or patch ? I search but i don't find anything actually.
best regards
Nicolas.
Solved! Go to Solution.
Are you working of the linux source code found at the below link:
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_2.6.35_11.09.01
I would recommend that you replicate the settings for UART3 found in serial.h for UART5.
Best regards,
-Mahesh
I have just given Freescale support a version of the mxc_uart.c driver containing a number of fixes for bugs in DMA operation at high baud rates. If you ask them nicely they should be able to provide it to you.
I am not sure what the clock issue was, but DMA was re-enabled on UART 3 via a subsequent patch that also increased the UART DMA RX buffer size. Below is the commit.
commit 191aff8468999abc730ffe4ee0b99fc6afd6a091
Author: Zhang Jiejing <jiejing.zhang@freescale.com>
Date: Fri Apr 1 10:33:26 2011 +0800
ENGR00140702-2 MX5: UART: enable UART3 DMA transfer
- enable DMA transfer of UART3
- enlarge DMA receive buffer size.
Signed-off-by: Zhang Jiejing <jiejing.zhang@freescale.com>
diff --git a/arch/arm/mach-mx5/serial.h b/arch/arm/mach-mx5/serial.h
index 9fbb0b3..6ed55da 100644
--- a/arch/arm/mach-mx5/serial.h
+++ b/arch/arm/mach-mx5/serial.h
@@ -51,8 +51,8 @@
#define UART2_UFCR_TXTL 16
/* UART 3 configuration */
#define UART3_UCR4_CTSTL 16
-#define UART3_DMA_ENABLE 0
-#define UART3_DMA_RXBUFSIZE 1024
+#define UART3_DMA_ENABLE 1
+#define UART3_DMA_RXBUFSIZE 2048
#define UART3_UFCR_RXTL 16
#define UART3_UFCR_TXTL 16
/* UART 4 configuration */
with those UART related patches merged, the issue still exists on UART3!how can I do to solve it?
This patch was cherry-picked from the 2.6.35_maintain branch to 11.09 branch. Below is the link:
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_2.6.35_maintain&ofs=50
Yes, I see that. However, I'm on the 2.6.35_maintain branch and am seeing the same error on UART3 (/dev/ttymxc2), which appears to be the only port with DMA enabled, but only if I get the data rate wrong:
~$ microcom -s 115200 /dev/ttymxc2
$C83.9P0.3R0.6T25.7*12
$C84.0P0.3R0.6T25.7*1C
$C84.0P0.3R0.6T25.7*1C
$C84.0P0.2R0.6T25.7*1D
$C84.0P0.2R0.6T25.7*1D
~$ microcom -s 9600 /dev/ttymxc2
[ 382.075133] UART: DMA_ERROR: sr1:2040 sr2:5089
�[ 382.106380] UART: DMA_ERROR: sr1:2040 sr2:5089
�[ 382.169261] UART: DMA_ERROR: sr1:2040 sr2:5089
�g�3�[ 382.263372] UART: DMA_ERROR: sr1:2040 sr2:5089
�?[ 382.326259] UART: DMA_ERROR: sr1:2040 sr2:5089
After looking at the code, this is expected on serial errors.
Hi Nicolas, did Mahesh's answer help you? If yes, please mark your DI as Correct Answer.
Are you working of the linux source code found at the below link:
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_2.6.35_11.09.01
I would recommend that you replicate the settings for UART3 found in serial.h for UART5.
Best regards,
-Mahesh
Hi,
Yes it's from git I take the kernel, three or four months ago.
I enabled the dma for uart5 in the same way of uart3.
Actually I am on another project for the week. The next week I do anther tests.
Best regards,
Nicolas
Please get the latest code from :
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_2.6.35_11.09.01
A recent patch was added to update UART SDMA scripts.
Best regards,
-Mahesh
I also met this issue in mx53 uart3: UART: DMA_ERROR: sr1:2040 sr2:508c
My uart3 connnect a bluetooth module, and only first DMAread operation occur this error, sequential DMAread successful.
I patch several commits including the one update UART SDMA scripts, but this error still occurs.
BTW, I noticed this git commit:
-------------------------------------------------------
commit a77a4c4f12640c414adf8c4381cb1d8eb8364dd0
Author: Zhang Jiejing <jiejing.zhang@freescale.com>
Date: Wed Dec 8 20:24:04 2010 +0800
ENGR00137669-3 MX53_SMD: workaround for UART have problem when DMA enable.
There is a clock issue when UART3 enable DMA, so disable this.
Signed-off-by: Zhang Jiejing <jiejing.zhang@freescale.com>
----------------------------------------------------
what's mean "a clock issue"? any detail?
BR
wenpeng
Is there any reason why this patch hasn't been applied to the imx_2.6.35_maintain branch yet?