iMX53 QSB - out of box boot failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX53 QSB - out of box boot failure

1,577 Views
AhmetYUCE
Contributor II
I've received an iMX53 QSB recently, sch Rev E. An microSD came within the package, labeled as "MX535START UBUNTU77347C L2.6.35_11.01ER". I believe its preloaded with Ubuntu. First put this SD into rugular SD slot with no luck, then into microSD card. So u-boot runs, kernel starts to load but hangs afler initializing USB. I haven't change any u-boot parameter. It's all stock SD. Where should i check? Any idea? Regards Ahmet
Labels (1)
0 Kudos
Reply
7 Replies

1,253 Views
SteveBakke
Contributor II

Did anyone solve this? I'm having the same problem.  Boots and last line displayed is:

"usbcore: registered new interface driver usb-storage"

Then appears to crash.

Tried with USB Key/mouse, no key/mouse, powered hub, .... same results.

0 Kudos
Reply

1,253 Views
thouswave
Contributor III

I have solve the problem,maybe can give you some advice.

PS:Power Consumption

First,I use a 5V-2A power source,imx53 boot fail after init usb.For the board will driver usb keyboard and mouse,and a VGA display,I considered if power is enough.

Then I use a 5V-4A power source,the board boot OK.

Theoretically,5V-2A is enough,but sometimes,power source's quality should be considered.

0 Kudos
Reply

1,253 Views
EugeneNekipelow
Contributor I

Same problem. With USB peripherals my board hangs up always.

Without peripherals the board hangs up 9/10.  :DDD

0 Kudos
Reply

1,253 Views
PhilEndecott
Contributor II
> lower USB port should be left unconnected Not necessarily. > I've attached a USB hub into the upper USB port and > connected mouse & keyboard it Right. For best results, use a powered hub. If you have an oscilloscope, watch the 5v rail as the system starts. The board has very little "tank" capacitance on its input. When the USB devices are turned on the power supply can "brown out".
0 Kudos
Reply

1,253 Views
AhmetYUCE
Contributor II
Found the problem, lower USB port should be left unconnected. I've attached a USB hub into the upper USB port and connected mouse & keyboard it.
0 Kudos
Reply

1,253 Views
AhmetYUCE
Contributor II
Only keyboard and mouse was connected to USB. Tried removing them, still locks. Boot messages are below. Hangs after the last line... ********************************************************************************************************** U-Boot 2009.08 (Mar 23 2011 - 12:37:0 CPU: Freescale i.MX53 family 2.1V at 1000 MHz mx53 pll1: 1000MHz mx53 pll2: 400MHz mx53 pll3: 216MHz mx53 pll4: 455MHz ipg clock : 66666666Hz ipg per clock : 33333333Hz uart clock : 21600000Hz cspi clock : 54000000Hz ahb clock : 133333333Hz axi_a clock : 400000000Hz axi_b clock : 200000000Hz emi_slow clock: 133333333Hz ddr clock : 400000000Hz esdhc1 clock : 80000000Hz esdhc2 clock : 80000000Hz esdhc3 clock : 80000000Hz esdhc4 clock : 80000000Hz nfc clock : 26666666Hz Board: MX53-LOCO Boot Reason: [POR] Boot Device: SD I2C: ready DRAM: 1 GB MMC: FSL_ESDHC: 0, FSL_ESDHC: 1 In: serial Out: serial Err: serial Net: got MAC address from IIM: 00:04:9f:01:e0:84 FEC0 [PRIME] Hit any key to stop autoboot: 0 MMC read: dev # 0, block # 2048, count 6144 partition # 0 ... 6144 blocks read: OK ## Booting kernel from Legacy Image at 70800000 ... Image Name: Linux-2.6.35.3-744-g27fdf7b Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2967420 Bytes = 2.8 MB Load Address: 70008000: _populate_mpu_rt_base f Entry Point: 70008000wkupror value 0xEE6C94 Verifying Checksum ... OK Loading Kernel Image ... OK NR_IRQS:409echo Runnin OK Starting kernel ...cking rate (Crystal Linux version 2.6.35.3-744-g27fdf7b (r80115@bluebell) (gcc version 4.4.4 (4.4.4_ i2c1: softreset failed (waited 10000 usec)mming SDRC clock to 400000000 Hzadadd 09.06.2010) ) #1 PREEMPT Thu Jan 27 15:10:16 CST 2011 CPU: ARMv7 Processor [412fc085] revision 5 (ARMv7), cr=10c53c7f[ 0.109802] omap_hwmod: i2c2: softreset failed (waited 10000 CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache IRQ: Found an INTC at 0xfa200000 (revision 4.0) w Machine: Freescale MX53 LOCO Board Memory policy: ECC disabled, Data cache writebackfailed (waited 10000 usec) Kernel command line: console=ttymxc0,115200 video=mxcdi1fb:GBR24,XGA di1_primary Trying to install inter [ 0.123840] NET: Registered p tve root=/dev/mmcblk0p1 rw rootwait stderr PID hash table entries: 4096 (order: 2, 16384 bytes) [ 0.124053] GPMC revis Dentry cache hash table entries: 131072 (order: 7, 524288 bytes) T [ 0.125213] OMAP GPIO har Inode-cache hash table entries: 65536 (order: 6, 262144 bytes) Memory: 352MB 512MB = 864MB totalardware version 2.551024MR-16@ Memory: 868260k/868260k available, 16476k reserved, 0K highmem26892] omap_mux_init: Add partition: #1: core, flags: 0ead Virtual kernel memory layout: 0x00000263 ** pkmap : 0x7fe00000 - 0x80000000 ( 2 MB) 0.132568] Unable to get DVI reset GPIOor value modules : 0x7f000000 - 0x7fe00000 ( 14 MB) ***** R Security Framework in .init : 0x80008000 - 0x80033000 ( 172 kB) debug architecture 0x4 unsupported.ries: 512 at .text : 0x80033000 - 0x807e9000 (7896 kB) .data : 0x80806000 - 0x8085a4e0 ( 338 kB)ting write b [ 0.135345] O MXC IRQ initialized MXC_Early serial console at MMIO 0x53fbc000 (options '115200') twl4030: gpio (irq 368) c ndbyng I bootconsole [ttymxc0] enablednstraints: VDAC: 1800 mV norm Console: colour dummy device 80x30ormal standbytdelay=1 init=/init i Calibrating delay loop... 999.42 BogoMIPS (lpj=4997120) pid_max: default: 32768 minimum: 301_constraints: VDVI: 1800 mV normal s Mount-cache hash table entries: 5 regulator: VS NET: Registered protocol family 16x Sound Architecture Driver Versio i.MX IRAM pool: 128 KB@0xe0840000 IRAM READY CPU is i.MX53 Revision 2.1 regulator: Using SDMA I.APIormal st MXC DMA API initialized [ 0.188873] NetL IMX usb wakeup probe IMX usb wakeup probeator: VAUX4: 1800 mV bio: create slab at 0 [ 0.188903] NetLabel: SCSI subsystem initialized Freescale USB OTG Driver loaded, $Revision: 1.55 $ worst case deact usbcore: registered new interface driver usbfss = UNLABELED CIPSOv4 usbcore: registered new interface driver hub0xffc omap_i2c omap_i2c.2 usbcore: registered new device driver usbbel: unlabeled traffic allowed regulator: DA9052_LDO4: 1725 <--> 3300 mV at 2775 mV normal 0x000002A9 [ 0.221435] UDP-Lite regulator: DA9052_LDO5: 1200 <--> 3600 mV at 1300 mV normal regulator: DA9052_LDO6: 1200 <--> 3600 mV at 1300 mV normal0.97 (double precisio regulator: DA9052_LDO7: 1200 <--> 3600 mV at 2750 mV normalamily 10x000002AC regulator: DA9052_LDO8: 1200 <--> 3600 mVisp regi VFS: Disk quotas dquot_6 regulator: DA9052_BUCK_PRO: 500 <--> 2075 mV at 1300 mV normal[ 0.222717] RPC: Registered tcp transport module.rder 0, 40 regulator: DA9052_BUCK_MEM: 925 <--> 2500 mV at 1500 mV normal regulator: DA9052_BUCK_PERI: 1800 <--> 3600 mV at 3600 mV normalckcD) (SUMMARY) 7.64 IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)init: 600000 bytes @ 9ee00000 Advanced Linux Sound Architecture Driver Version 1.0.23.erial: 8250/16550 driver, 4 ports, IRQ s Bluetooth: Core ver 2.15 Bluetooth: HCI socket layer initialized [ 0.594787] type= Switching to clocksource mxc_timer1 NET: Registered protocol family 2 omap_uart.1: IP route cache hash table entries: 32768 (order: 5, 131072 bytes)quotas dquot_6.5.2O hardware version 2.5 TCP established hash table entries: 131072 (order: 8, 1048576 bytes)e hash table entries: 1024 (order 0, 4096 bytes)UART2_init: Add part TCP bind hash table entries: 65536 (order: 6, 262144 bytes) TCP: Hash tables configured (established 131072 bind 65536)755981] Registering unionfs 2.5.9 (for 2.6.39-rc5)tyO3 at M TCP reno registered= 80) UDP hash table entries: 512 (order: 1, 8 RPC: Registered tcp NFSv4.1 backchannel transport module. [ 1.637817] LPMode driver module loadedehci-omap.0: OMAP-EHCI Host Static Power Management for Freescale i.MX5 [ PM driver module loadedttyO3 at MMIO 0x4904200 sdram autogating driver module loadedegistered, assigned bus number 1tandb Bus freq driver module loaded DI1 is primary mxc_dvfs_core_probe DVFS driver module loaded [ 1.655120] b i.MXC CPU frequency driverci-omap.0: irq 77, io m DVFS PER driver module loaded msgmni has been set to 1695river initializing alg: No test for stdrng (krng) 0x000002DC error value 0 cryptodev: driver loaded. regulator: VAUX4 io scheduler noop registeredNAND device found.ndor=1d6b, io scheduler deadline registered io scheduler cfq registered (default)5567] No NAND device found.ate latenc mxc_ipu mxc_ipu: Channel already disabled 9 usb usb1: New USB devi mxc_ipu mxc_ipu: Channel already uninitialized 9zingFF IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)CP reno usb u [ 3.766479] hub 1-0:1.0 Console: switching to colour frame buffer device 128x48 TVE as primary display [ 3.770477] hu mxc_ipu mxc_ipu: Channel already disabled 9: Serial: MXC Internal UART driverer gadget: using random self eth mxcintuart.0: ttymxc0 at MMIO 0x53fbc000 (irq = 31) is a Freescale i.MX f_mass_storage inited 0xCFDCDCE8 console [ttymxc0] enabled, bootconsole disableddget: using random host ethernet addressche has console [ttymxc0] enabled, bootconsole disable 0x000003 mtdo [ 3.891784] mxcintuart.3: ttymxc3 at MMIO 0x53ff0000 (irq = 13) is a Freescale i.MX [ scsi0 : ahci ata1: SATA max UDMA/133 mmio [mem 0x10000000-0x10000fff] port 0x100 irq 28 MXC MTD nand Driver 3.0 i.MX GPMI NFC vcan: Virtual CAN interface driver Freescale FlexCAN Driver FEC Ethernet Driver fec_enet_mii_bus: probed ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1 fsl-ehci fsl-ehci.0: irq 18, io base 0x53f80000 fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2 fsl-ehci fsl-ehci.1: irq 14, io base 0x53f80200 fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00 hub 2-0:1.0: USB hub found hub 2-0:1.0: 1 port detected Initializing USB Mass Storage driver... usbcore: registered new interface driver usb-storage
0 Kudos
Reply

1,253 Views
PhilEndecott
Contributor II
> hangs afler initializing USB. Do you have things plugged into the USB sockets? Try unplugging them.
0 Kudos
Reply