Hi,
I have iMX53 QSB.
I have downloaded Ubuntu VM from freescale site. Along with it a pre-built image for iMX53 QSB board is available.
So with the help of manual I burn this image (ubuntu_start_board.bin) into 4GB SD Card with help of following command
sudo dd if=/home/lucid/Desktop/ubuntu_start_board.bin of=/dev/sdb
But I am getting following error can't get kernel image!.
Please help me regarding same. Am I missing anything while following document. I am attaching document with this post.
U-Boot 2009.08 (Oct 20 2011 - 13:11:26)
CPU: Freescale i.MX53 family 2.1V at 800 MHz
mx53 pll1: 800MHz
mx53 pll2: 400MHz
mx53 pll3: 432MHz
mx53 pll4: 455MHz
ipg per clock : 33333333Hz
uart clock : 66666666Hz
cspi clock 108000000Hz
ahb clock 133333333Hz
axi_a clock : 400000000Hz
axi_b clock : 200000000Hz
emi_slow clock:da9052_i2c_is_connected - i2c write success....
Serial reinitilized!
Net: got MAC address from IIM: 00:04:9f:01:db:da
FEC0 [PRIME]
Hit any key to stop autoboot: 0
MMC read: dev # 0, block # 2048, count 6144 ... Card did not respond to voltage select!
MMC: block number 0x2000 exceeds max(0x0)
0 blocks read: ERROR
Wrong Image Format for bootm command
ERROR: can't get kernel image!
Following is log from printenv:
baudrate=115200
loadaddr=0x70800000
netdev=eth0
ethprime=FEC0
uboot=u-boot.bin
kernel=uImage
ethact=FEC0
bootcd=run bootcmd_mmc
bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm
bootcmd_mmc=run bootargs_base bootargs_mmc; mmc read ${loadaddr} 0x800 0x1800; bootm
bootargs_mmc=set bootargs ${bootargs} root=/dev/mmcblk0p1 rw rootwait
vga=setenv bootargs console=ttymxc0,115200 video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga
bootcmd_obds=ext2load mmc 0:1 0x70800000 /unit_tests/obds.bin; go 70800000
nfsroot=/tftpboot/rootfs
lcd=video=mxcdi0fb:RGB24,SEIKO-WVGA di0_primary
lvds=video=mxcdi0fb:RGB666,XGA di0_primary ldb=di0
bootcmd=run bootcmd_mmc
bootfile=uImage
fileaddr=70800000
netmask=255.255.254.0
hdmi=setenv bootargs console=ttymxc0,115200 video=mxcdi0fb:RGB24,1024x768M@60 hdmi di0_primary
serverip=192.168.0.1
ipaddr=192.168.0.2
gatewayip=192.168.0.1
bootargs_base=setenv bootargs console=ttymxc0,115200 gpu_nommu ${vga}
dnsip=192.168.0.1
bootdelay=3
stdin=serial
stdout=serial
stderr=serial
bootargs=console=ttymxc0,115200 gpu_nommu setenv bootargs console=ttymxc0,115200 video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga root=/dev/mmcblk0p1 rw rootwait
Environment size: 1289/8188 bytes
Thanks in advance.
Raj Sanghavi
According to the message from the log
"MMC read: dev # 0, block # 2048, count 6144 ... Card did not respond to voltage select!"
there is no proper card inserted to SD port 0.
Is Your SD card located there (in slot 0) ?
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Yuri,
Thanks for valuable reply.
I changed dev #0 to dev #1 and my board just started working as of now.
I used following command to do this thing
setenv bootcmd_mmc 'run bootargs_base bootargs_mmc; mmc dev 1;mmc read ${loadaddr} 0x800 0x1800; bootm'
bootargs=console=ttymxc0,115200 gpu_nommu setenv bootargs console=ttymxc0,115200 video=mxcdi0fb:RGB24,1920x1080M@60 hdmi di0_primary root=/dev/nfs ip=dhcp nfsroot=10.2
9.240.144:/tftpboot/rootfs,v3,tcp
setenv bootargs 'console=ttymxc0,115200 gpu_nommu ${lvds}'
Though my board is booting now, to understand things correctly can you please guide me why I have to change dev #0 to dev#1 and what these above command needed.
Thanks in advance.
Raj sanghavi