iMX53 QSB CE7 not being detected by Windows Mobile Device Center

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX53 QSB CE7 not being detected by Windows Mobile Device Center

跳至解决方案
1,599 次查看
JD1z
Contributor II

Hi All

I'm just back working on a iMX3 QSB (Compact 7) after 6 months of other work. The problem I have is that the QSB is not being detected by the Windows Mobile Device Center(WMDC) and so cannot connect to it from Visual Studio 2008. This was all working fine before.

Nothings changed as far as the uSD card is concerned.

I've tried reinstalling WMDC, this is on a Windows 7 32 bit PC so cannot use ActiveSync.

I had wondered whether an update to Windows 7 had caused this to stop working, hence the reinstall of WMDC.

I cannot see any changes to the list in Device Manager while I plug and unplug the USB cable.

I've tried:-

     different USB cables.

     one of the othe QSB's we have in the office, with no luck

     the Ubuntu uSD card that came with the kit.

     Installing WMDC on a different PC and again nothing, not even a notification or anything in Device Manager

Has anybody had any similar issues? Any help in resolving this is much appreciated, cannot do aything until this is resolved.

Thanks

Jaswinder

标签 (1)
0 项奖励
回复
1 解答
1,289 次查看
JD1z
Contributor II

Ok, got this working.

Used a USB analyser to see if the QSB was sending anything to he PC...Nothing.

So the problem was with the QSB.

I noticed that double-clicking the "USB Serial" icon in [ControlPanel->Network and Dial-up Connections->USB Serial] gave me an error.

Hoping it wasn't a hardware problem, I used CFimager to make another SDCard and all was well again.

Regards

Jaswinder

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,290 次查看
JD1z
Contributor II

Ok, got this working.

Used a USB analyser to see if the QSB was sending anything to he PC...Nothing.

So the problem was with the QSB.

I noticed that double-clicking the "USB Serial" icon in [ControlPanel->Network and Dial-up Connections->USB Serial] gave me an error.

Hoping it wasn't a hardware problem, I used CFimager to make another SDCard and all was well again.

Regards

Jaswinder

0 项奖励
回复