iMX53 QSB CE7 not being detected by Windows Mobile Device Center

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX53 QSB CE7 not being detected by Windows Mobile Device Center

ソリューションへジャンプ
1,589件の閲覧回数
JD1z
Contributor II

Hi All

I'm just back working on a iMX3 QSB (Compact 7) after 6 months of other work. The problem I have is that the QSB is not being detected by the Windows Mobile Device Center(WMDC) and so cannot connect to it from Visual Studio 2008. This was all working fine before.

Nothings changed as far as the uSD card is concerned.

I've tried reinstalling WMDC, this is on a Windows 7 32 bit PC so cannot use ActiveSync.

I had wondered whether an update to Windows 7 had caused this to stop working, hence the reinstall of WMDC.

I cannot see any changes to the list in Device Manager while I plug and unplug the USB cable.

I've tried:-

     different USB cables.

     one of the othe QSB's we have in the office, with no luck

     the Ubuntu uSD card that came with the kit.

     Installing WMDC on a different PC and again nothing, not even a notification or anything in Device Manager

Has anybody had any similar issues? Any help in resolving this is much appreciated, cannot do aything until this is resolved.

Thanks

Jaswinder

ラベル(1)
0 件の賞賛
返信
1 解決策
1,279件の閲覧回数
JD1z
Contributor II

Ok, got this working.

Used a USB analyser to see if the QSB was sending anything to he PC...Nothing.

So the problem was with the QSB.

I noticed that double-clicking the "USB Serial" icon in [ControlPanel->Network and Dial-up Connections->USB Serial] gave me an error.

Hoping it wasn't a hardware problem, I used CFimager to make another SDCard and all was well again.

Regards

Jaswinder

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,280件の閲覧回数
JD1z
Contributor II

Ok, got this working.

Used a USB analyser to see if the QSB was sending anything to he PC...Nothing.

So the problem was with the QSB.

I noticed that double-clicking the "USB Serial" icon in [ControlPanel->Network and Dial-up Connections->USB Serial] gave me an error.

Hoping it wasn't a hardware problem, I used CFimager to make another SDCard and all was well again.

Regards

Jaswinder

0 件の賞賛
返信