iMX53 QSB 640x480?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX53 QSB 640x480?

914件の閲覧回数
yvan
Contributor II

Hello,

 

I'm trying to use a 640x480 LVDS screen on my mx53QSB.

So I added 

         /* 640x480 @ 60 Hz, 31.5 kHz hsync */

        { "VGA", 60, 640, 480, 39721,

        40, 24,

        32, 11,

        96, 2,

         0,

        FB_VMODE_NONINTERLACED,

        0,},

in video_modes[] of arch/arm/mach-mx5/mx53_loco.c

recompiled...

 

Then I changed my uBoot env

lvds=mxcdi0fb:RGB666,VGA ldb

instead of

lvds=mxcdi0fb:RGB666,XGA ldb

 

And... I've got nothing on the screen

 

Note : When using XGA the screen is working (with a cropped image of course)

 

What am I missing? 

タグ(1)
0 件の賞賛
2 返答(返信)

681件の閲覧回数
LilyZhang
Contributor I

Yes. Please ensure you also add relative mode into drivers/video/mxc/ldb.c.

Please also check the clock configurations in ldb.c and ensure it can support your panel

0 件の賞賛

681件の閲覧回数
yvan
Contributor II

Ok! just found it!

We also need to add this new mode in :

drivers/video/mxc/ldb.c

0 件の賞賛