iMX53 PCB impedance control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX53 PCB impedance control

Jump to solution
1,234 Views
kamejoko80
Contributor II
Hi all, I wan to reuse the iMX53 QSB-R PCB stack up in oder to design a new custome board, but I don't known detail of the stack up such as PCB thickness and the dielectric thickness for each layer... I saw there are some different point between the allegro PCB design board stackup and the detail information from their gerber files. Which is correct that I should follow and ask the PCB manufacturer for PCB impedance controlling? Any suggestions ? Best regard
Labels (1)
0 Kudos
1 Solution
812 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Minh,

 

The MX53 QSB-R PCB is compliant with IPC-A-600 Class 2, this standard specifies board thickness. The stackup of the board, which specifies the layer thickness, is included in the layout. I'm attaching a PDF of the stackup and fab notes, these include everything you need. Unfortunately, I don't have the IPC-A-600 document, but this is something your manufacturer must know, so they can provide some guidance about it.

 

Best regards.

Jorge.

View solution in original post

0 Kudos
3 Replies
812 Views
TheAdmiral
NXP Employee
NXP Employee

Hi Minh,

Always follow the recommendations fo the PCB manufacturer. Each manufacturer has a different process and different set of materials. And the materials used may vary depending on what the manufacturer has on hand. Give the manufacturer some tartget values for: overall thickness, number of layers, and desired trace impedances. Ask them to provide to you a recommended board stack up and trace thicknesses. Then use these in your design. The initial stackup information provided by the manufacturer for the Freescale QuickStart board is contained in chapter 8 of the Hardware Reference Manual for i.MX53 Quick Start (available for download from Freescale).

Cheers.

813 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Minh,

 

The MX53 QSB-R PCB is compliant with IPC-A-600 Class 2, this standard specifies board thickness. The stackup of the board, which specifies the layer thickness, is included in the layout. I'm attaching a PDF of the stackup and fab notes, these include everything you need. Unfortunately, I don't have the IPC-A-600 document, but this is something your manufacturer must know, so they can provide some guidance about it.

 

Best regards.

Jorge.

0 Kudos
812 Views
NicolasIzquierd
Contributor III

Hi Phuong

As you mention, Inside the Gerbers Files and the Layout file as well, there is a table named "IMPEDANCE REQUIREMENTS" together with the PCB Material and the weigh of copper for each layer from the StackUp, you should with your PCB Manufacturer agreed in to match as close as possible to get these impedance in your traces, and define the proper thickness of you pcb.

hope this can help you.

-ni