On page 1774 of the iMX53 Reference Manual rev 2.1 dated 6/2012, the following line is at the bottom of the page (in paragraph 39.12.1, AHB Slave Interface):
Description of all user-accessible registers in the design can be found from regs.html
Where can I get a copy of regs.html?
Hi Neil
unfortunately this file is not available since it is property
of gpu owner (amd).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Are you kidding? Freescale sells processors without the information necessary to use them???
Hi Neil
suggest to contact local FAE to obtain more details.
This gpu module is third party IP so info
about it and detailed documentation its registers is license protected.
Freescale provides gpu libraries in binary forms only for
customer usage. For gpu programming OpenGL ES/OpenVG APIs
are used. You can look for examples below
IMX_GPU_SDK 
 : Linux GPU SDK
Chapter 16 Graphics Processing Unit (GPU)
mx53_start_linux.pdf
Best regards
igor
Igor,
Thank you for the information. Unfortunately, binary libraries won't do us any good since we are using the processor in an avionics system. The FAA prohibits the use of binary libraries in flight software (see their position paper CAST-21 for details).
- Neil