Hi all,
iMX51 + WinEC700.
The BSP is based on the BSP from Freescale.
Sometimes happens that at the OS start - after the bootloader - the screen stays blank (especially if i'm running with the batteries, with the wall charger i never see that).
If I check on the debug log i see the following:
1. correct
..
OSC = 24000000 Hz
CKIH_CAMP1 = 22579200 Hz
CKIH2_CAMP2 = 0 Hz
CKIH2 = 0 Hz
FPM = 33554432 Hz
Windows CE Kernel for ARM (Thumb Enabled)
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb
OEMInit: silicon€’•Ùê‚ÂÉ‚j¤$ê+–V)¤‚ÂÁrj¤tJåJzÅj*‹+Ê+‹—Z•EÅ
‰TkW–,«V¨HøPID:00400002 TID:00510002 OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)
PID:00400002 TID:00510002 WARNING: SRTC was reset.
PID:00400002 TID:009F0006 IpuBufferManagerInit(): Detected reserved video memory(67108864 bytes), will ignore registry setting!
PID:00400002 TID:009F0006 BSPGetPercentOfPowerCapability 35% 3570mV
PID:00400002 TID:009F0006 - in=35 ret=35
PID:00400002 TID:009F0006 +BSPBacklightInitialize
PID:00400002 TID:009F0006 +BSPBlSetInt 255
VBridge:: VB_INITIALIZED returns [0]
PID:00400002 TID:02EE0002 UsbHost : New Hub [address(1) / layer(0)]
PID:00400002 TID:03D1000E UsbHost : New Function [address(2) / layer(1)]
PID:00400002 TID:046C0006 +BSPInitializePanel portID=4 'LVDS 1024x768 Tianma'
PID:00400002 TID:046C0006 --++++++--
PID:05990016 TID:055A0032 MBS: DllMain(1)
PID:00400002 TID:03D1000E UsbHost : New Function [address(3) / layer(1)]
PID:00400002 TID:03D1000E USBHost : Detach Function [address(2) / layer (1)]
PID:05220036 TID:05240036 +FileEsists \SDMemory\Reboot\Delete\UpdDel.inf
PID:05220036 TID:05240036 -FileExist err=3
PID:05220036 TID:05240036 +DirEsists \SDMemory\Reboot\Copy\
PID:05220036 TID:05240036 (startup) Check registry backup
PID:00400002 TID:01DA0072 - in=35 ret=35
PID:055B005A TID:05AD005A CP_UTF8 Supported
PID:00400002 TID:01DA0072 - in=35 ret=35
PID:00400002 TID:05AD005A +BSPBlSetInt 255
PID:00400002 TID:05AD005A +BSPBlSetInt 255
PID:00400002 TID:05AD005A - in=35 ret=35
PID:055B005A TID:04CE0086 CP_UTF8 Supported
PID:055B005A TID:04B5009E CP_UTF8 Supported
PID:055B005A TID:04FF00A2 CP_UTF8 Supported
PID:00400002 TID:05AD005A - in=35 ret=35
PID:055B005A TID:053400A2 CP_UTF8 Supported
PID:00400002 TID:05AD005A - in=35 ret=35
PID:00400002 TID:01DA0072 - in=35 ret=35
PID:055B005A TID:051C00A6 CP_UTF8 Supported
PID:055B005A TID:051C00A6 [SDI]: Start device init
PID:00400002 TID:05AD005A - in=35 ret=35
...
The screen is initialized between the USB detections (always..).
When I have the blank screen the log is:
...
OSC = 24000000 Hz
CKIH_CAMP1 = 22579200 Hz
CKIH2_CAMP2 = 0 Hz
CKIH2 = 0 Hz
FPM = 33554432 Hz
Windows CE Kernel for ARM (Thumb Enabled)
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb
OEMInit: silicon€’•Ùê‚ÂÉ‚j¤$ê+–V)¤‚ÂÁrj¤tJåJzÅj*‹+Ê+‹—Z•EÅ
‰TkW–,«V¨Hø PID:00400002 TID:00510002 OALIoCtlHalInitRTC(2006/1/1 12:0:0.000)
PID:00400002 TID:00510002 WARNING: SRTC was reset.
PID:00400002 TID:009F0006 IpuBufferManagerInit(): Detected reserved video memory(67108864 bytes), will ignore registry setting!
PID:00400002 TID:009F0006 BSPGetPercentOfPowerCapability 40% 3585mV
PID:00400002 TID:009F0006 lim min=35
PID:00400002 TID:009F0006 - in=40 ret=35
PID:00400002 TID:009F0006 +BSPBacklightInitialize
PID:00400002 TID:009F0006 +BSPBlSetInt 255
VBridge:: VB_INITIALIZED returns [0]
PID:00400002 TID:02E90002 UsbHost : New Hub [address(1) / layer(0)]
PID:00400002 TID:03E10006 UsbHost : New Function [address(2) / layer(1)]
PID:00400002 TID:03E10006 UsbHost : New Function [address(3) / layer(1)]
PID:00400002 TID:01DA0072 - in=40 ret=35
PID:00400002 TID:01DA0072 - in=40 ret=35
PID:00400002 TID:01DA0072 BSPGetPercentOfPowerCapability 35% 3561mV
PID:00400002 TID:01DA0072 - in=35 ret=35
PID:00400002 TID:01DA0072 - in=35 ret=35
...
That means that the LCD driver (and the next apps) is not loaded but i don't know why???
Any idea?
Can you disable the USB driver and have a try?
Do you mean to disable the USB item in the catalog?
No, for the moment ..
Yes. You can remove the USB drivers in the catalog to check if the usb driver impacted the LCD.
Ok, but i don't know if the USB driver is the culprit: this is the best clue i have, so far.
After some negative consecutive tests (that is, blank screens) I deleted the /Registry/system.hv file.
After that the system was able to start (?!?!?!?!?!?).
I don't really understand how it is possible: seems the registry is corrupted .. but the applications are not running.
Did you enable the HIV registry?
Yes
Maybe it doesn't use the new HIV registry? I am not sure. You can check it.