iMX51 and boundary scan

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX51 and boundary scan

2,026 次查看
allians-spb
Contributor I

When connected via JTAG, 3 devices are detected. Using TOPJTAG! Two devices are known - the i MX51 chip itself and the core! The third device is identified with ID=0, most likely it is SDMA! IR length?

标签 (1)
0 项奖励
回复
4 回复数

1,883 次查看
allians-spb
Contributor I

Thanks!!! Now you can control the legs!!! And there is only one device - iMX51!

0 项奖励
回复

1,883 次查看
allians-spb
Contributor I

JTAG_MOD и так подтянут к GND! JTAG работает, только программа находит неизвестное устройство с ID=0 и отказывается работать!

JTAG_MOD and so pulled up to GND! JTAG works, only the program finds an unknown device with ID=0 and refuses to work!

0 项奖励
回复

1,883 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sergei

I am very sorry, correct is : JTAG_MOD should be high for bsdl.

Best regards
igor

0 项奖励
回复

1,883 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sergei

JTAG_MOD should be high for bsdl, when low one can see chain

similar to Figure 8-3. i.MX/Cortex-A8 RVDS JTAG Scan Chain

i.MX53 System Development User’s Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复