iMX357 booting issue and manual reset not working.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX357 booting issue and manual reset not working.

1,600 次查看
naushad
Contributor I

I am using iMX357 processor along with MC13892AJVL, 256Mbyte DDR2 and 256MByte NAND Flash. The board was working very good for 6months, but after that some irregular behavior started:

1. In some cases the processor is not booting when Power supply  turned ON. In close observation we found that this is happening when the power OFF to ON time is very less(approximately 2 seconds or less).

 

2. In some cases the processor not booting immediately but after a few seconds only( approximately 1 or 2 seconds)

 

3. Manual reset connected to RESET_IN_B pin was working perfectly earlier but it stopped working now.

 

All these issues started after a time of 6months. During this time the board was working perfectly and we were developing some application software.

 

Please let me know if anybody have experience in the same or any idea about these issues?

0 项奖励
回复
2 回复数

1,212 次查看
Antman81
Contributor I

I have a product I’d like to repair which has this processor, and had the same symptoms. Not won’t boot at all. Was there a resolution to this?

0 项奖励
回复

1,475 次查看
freescale_dude
Contributor II

You need to ask this question in http://imxcommunity.org, which is where i.MX support is given.

 

---Tom

0 项奖励
回复