iMX28X_EVK board not detecting in Windows 7 64-bit System

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX28X_EVK board not detecting in Windows 7 64-bit System

902 Views
bkpatel
Contributor III

Hi,

I am trying to connect my iMX28 board with windows 7 64-bit system but device is not showing in Device Manager.

While connecting to Windows 8 it is showing under Human Interface Device (HID) List. Same is not available in Windows7.

How to connect to Windows 7?

Want to upload kernel and rootfs via MfgTool.

Thanks,

Bhavesh

Labels (3)
0 Kudos
Reply
1 Reply

711 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bhavesh

please try solutions provided on

Mfgtool can't connect in windows7

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply