iMX280 : i.MX28 EVK Board JTAG interface circuit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX280 : i.MX28 EVK Board JTAG interface circuit

ソリューションへジャンプ
1,392件の閲覧回数
koichisakagami
Contributor II

Dear community,

I am checking the i.MX28 EVK Board schematic (IMX28_evk_revD) .
It seems that the JTAG interface circuit is very complex.

If I execute the only simple Debugging ,  can the JTAG POD connect to i.MX jtag pin directly ?

Best Regards,
Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
1,114件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi koichi

yes, it can be connected directly.

FETs prevent backdrive from the JTAG interface.  Without these,

customers often complain that they either don’t see good power

numbers at low power states or they have difficulty getting repeatable power measurements.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,115件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi koichi

yes, it can be connected directly.

FETs prevent backdrive from the JTAG interface.  Without these,

customers often complain that they either don’t see good power

numbers at low power states or they have difficulty getting repeatable power measurements.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信