iMX280 : EMI Input voltage low (VLI) value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX280 : EMI Input voltage low (VLI) value

Jump to solution
1,519 Views
koichisakagami
Contributor II

Dear community,

I am checking the i.MX28 Data Sheet (IMX28CEC Rev3 07/2012) .
Please see Table 22 EMI Digital Pin DC Characteristics.
It says that the VIL value is 0.3V .

I think that the VIL value is -0.3V.

Which is correct ?

Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
Reply
1 Solution
1,430 Views
igorpadykov
NXP Employee
NXP Employee

Hi koichi

sorry, I misunderstood original question,

yes you are right in original post that correct reading

would be:

VIL value is -0.3V (Min.)

Best regards

igor

View solution in original post

0 Kudos
Reply
3 Replies
1,430 Views
igorpadykov
NXP Employee
NXP Employee

Hi koichi

correct is VIL value is 0.3V (Min.)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,430 Views
koichisakagami
Contributor II

Dear igor san,

Thank you for your reply.

As the VIL value is 0.3V ( Min),

it is not recognized that the Zero Voltage input is the Logical Low.

Is my understanding correct ?

Best Regards,

Koichi Sakagami

0 Kudos
Reply
1,431 Views
igorpadykov
NXP Employee
NXP Employee

Hi koichi

sorry, I misunderstood original question,

yes you are right in original post that correct reading

would be:

VIL value is -0.3V (Min.)

Best regards

igor

0 Kudos
Reply