iMX28 run openswan-2.6.18 problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX28 run openswan-2.6.18 problem

779件の閲覧回数
kevinyeh
Contributor I

Hi,all

I use LTIB L2.6.35_10.12.01 to build package openswan-2.6.18

I want to run ipsec protocol in iMX28 platform,but in the process of running openswan i got a problem and  need help:

   When i excute ipsec setup start,openswan needs about 5~7 minutes to create a connection,it's so slowly and very strange.

   Why the openswan need a lot of time to create a ipsec connection?

   I use two virtual machines run centOS5, compile openswan-2.6.18 with same sourece to test,but it create a connection very fast

   So i compile newer version of openswan to test,i try version 2.6.26 and 2.6.38 and get same problem

P.S I use wireshark to capture packets

Does anyone can give me some suggestion or solution?

ラベル(2)
タグ(1)
0 件の賞賛
返信
0 返答(返信)