Hello
We’re trying to enable the SPI functionality in an iMX287 with kernel 3.10.
We’ve added the highlighted lines to the imx28-mba28.dts file:
apb@80000000 {
apbh@80000000 {
pinctrl@80018000 {
...
};
};
apbx@80040000 {
ssp2: ssp@80014000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx28-spi";
pinctrl-names = "default";
pinctrl-0 = <&spi2_pins_a>;
status = "okay";
flash: m25p80@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "m25p80,fsl,imx28-spi";
spi-max-frequency = <40000000>;
reg = <0>;
};
};
};
};
But we’ve found that unless we comment the following highlighted lines in the imx28.dtsi file the compilation fails:
apb@80000000 {
apbh@80000000 {
compatible = "simple-bus";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x80000000 0x3c900>;
ranges;
/*ssp2: ssp@80014000 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x80014000 0x2000>;
interrupts = <98 84>;
clocks = <&clks 48>;
dmas = <&dma_apbh 2>;
dma-names = "rx-tx";
fsl,ssp-dma-channel = <2>;
status = "disabled";
};*/
pinctrl@80018000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx28-pinctrl", "simple-bus";
reg = <0x80018000 0x2000>;
spi2_pins_a: spi2@0 {
reg = <0>;
fsl,pinmux-ids = <
0x2100 /* MX28_PAD_SSP2_SCK__SSP2_SCK */
0x2110 /* MX28_PAD_SSP2_MOSI__SSP2_CMD */
0x2120 /* MX28_PAD_SSP2_MISO__SSP2_D0 */
0x2130 /* MX28_PAD_SSP2_SS0__SSP2_D3 */
>;
fsl,drive-strength = <1>;
fsl,voltage = <1>;
fsl,pull-up = <1>;
};
};
apbx@80040000 {
compatible = "simple-bus";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x80040000 0x40000>;
ranges;
};
};
};
Once we comment these lines the compilation is successfully completed but when booting the system we get the following error:
mxs-spi: probe of ssp.5 failed with error -22
Are we missing anything? Could you help us, please?
Thanks in advance for your help.
已解决! 转到解答。
Hi,
You can also check the binding documentation.
https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git/tree/Documentation/devicetree/b...
Alejandro
Hi,
You can also check the binding documentation.
https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git/tree/Documentation/devicetree/b...
Alejandro
Hi Silvia,
The compatible string you use is not correct.
Take a look at this dts file that shows the usage of a m25p80 spi flash on mx28: