Hi
I am writing some C code to set up and use AUART_0. through /dev/ttySP0. I am opening the port successfully and, when I write the port I am am actually getting data on the TX pin but then I get the following error: "mxs-auart mxs-auart.0: Unhandled status 52028d".
Any ideas are greatly appreciated!
Got it working! Avinash is right, these error codes appear to be associated with parity errors, framing errors, etc and I cannot find them documented anywhere either. My code is similar to Marcos except I'm not calling ioctl().
Also, I was not sending an LFCR after the string I was trying to send to my modem i.e. "ATZ\r\n" so now wonder I wasn't getting anything back!
I also faced similar problem, the errors messages was printed when I use parity, it would no appears if I didn't use parity.
Can you write your code for open the com port?
I use this:
/* open UART */
 if ((I_uart_file = ::open(device, O_RDWR | O_NOCTTY | O_NDELAY)) == -1) {
 /*
 * Could not open the port.
 */
 I_isOpen = P_Error;
return;
 }
 /* set BAUDRATE */
 tcgetattr(I_uart_file, &termios_old);
 termios_mxc = termios_old;
 termios_mxc.c_lflag &= ~(ICANON | ECHO | ISIG);
 cfsetospeed(&termios_mxc,B115200);
 cfsetispeed(&termios_mxc,B115200);
 retval = tcsetattr(I_uart_file, TCSANOW, &termios_mxc);
 line_val = LOOPBACK;
ioctl(I_uart_file, TIOCMSET, &line_val);
and I don't have any problem.
I also faced similar problem. I was getting the error code as 52080. Searched a lot in various documents, but could not find.
Practically I foound that these error codes are for parity error, framing error etc.