iMX28 : PWM output pin behavior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX28 : PWM output pin behavior

跳至解决方案
1,282 次查看
koichisakagami
Contributor II

Dear community,

We design the custom board .
We need information about PWM output pin behavior.

After the PWM register setting is completed,
we disable a PWM channel_xx by the PWM Control and Status Register (:PWMxx_ENABLE => 0).

Question1.
Then, What is the PWM output state ?
Is it high impedance ?

Question2.
    Then, Can the internal keeper be enabled / disabled separately ?

Best Regards,
Koichi Sakagami

标签 (1)
0 项奖励
回复
1 解答
1,180 次查看
igorpadykov
NXP Employee
NXP Employee

Hi koichi

1. yes it is high impedance

2. this can be done for some pads (not all), check

HW_PINCTRL_PULLx register descriptions.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,181 次查看
igorpadykov
NXP Employee
NXP Employee

Hi koichi

1. yes it is high impedance

2. this can be done for some pads (not all), check

HW_PINCTRL_PULLx register descriptions.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复