iMX28 Ethernet controller issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX28 Ethernet controller issue

3,458 次查看
jrtigerlee
Contributor III

I enable my Ethernet eth0 and eth1 to communication ,

then plug in-out on eth0 will reset eth1 and vice versa,

that I found docs from https://community.freescale.com/docs/DOC-94983 to explain this issue.


So I masked this GPIO reset function in fec_restart() on fec.c ,

And then plug in-out eth0/eth1 cable test again.


I found another critical issue , in fec_restart() function ,

when I write MAC0 register FEC_ECNTRL(HW_ENET_MAC_ECR) reset bit ,

both eth0 and eth1 will also be reset and the communication will be interrupted.

And if i write MAC0 register FEC_R_CNTRL(HW_ENET_MAC_RCR) RMII_MODE bit to disable,

both eth0 and eth1 will also be reset again.

But when I write this two register from MAC1 , it will not affect eth0


Does anyone have the same issue ?


标签 (2)
标记 (3)
6 回复数

2,780 次查看
ayazshahid
Contributor I

I have the same issue. Did you get a word from Freescale? Have they tagged it as an errata?

0 项奖励
回复

2,780 次查看
jrtigerlee
Contributor III

Hi Ayaz :

No , Freescale told to me to post this issue to community.

But seems no one can answer this

2,780 次查看
YixingKong
Senior Contributor IV

Jrtiger

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 项奖励
回复

2,780 次查看
YixingKong
Senior Contributor IV

Jrtiger

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel

free to reply with an update to this discussion.

Thanks,
Yixing

0 项奖励
回复

2,780 次查看
ayazshahid
Contributor I

Well tough luck for us then. Thanks for getting back to me

Cheers!

0 项奖励
回复

2,780 次查看
DuanFugang
NXP Employee
NXP Employee
0 项奖励
回复