iMX233 boot from SPI flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX233 boot from SPI flash

跳至解决方案
4,433 次查看
PotatoChip
Contributor I

Dear all,

I am trying to boot from SPI flash on imx233. I prepared a sb file with bootlet and kernel and programmed it to a SPI flash. The SPI flash is connected to SPI1.

I already set boot mode to boot from SPI1, but I get

0x80502008

     H0x80501003

I wonder if someone can give me any advise on it.

Regards,

JJ

0 项奖励
回复
1 解答
3,311 次查看
Yuri
NXP Employee
NXP Employee

Note, i.MX23 SPI bootloader supports only 2-byte addresses for EEPROMs and 3-byte addresses for NORs.

Next, please check if optional configuration block is located (and correct) at byte address 0, as described
in section 35.6.1 (Media Format) of the i.MX23 Reference Manual.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,311 次查看
PotatoChip
Contributor I

I programmed .sb file to a spi flash programmer and other thread said that program sb file to address 0x00 is what needed to be done. I don't know why it give 0x80501003 error. Any suggestion?

0 项奖励
回复
3,312 次查看
Yuri
NXP Employee
NXP Employee

Note, i.MX23 SPI bootloader supports only 2-byte addresses for EEPROMs and 3-byte addresses for NORs.

Next, please check if optional configuration block is located (and correct) at byte address 0, as described
in section 35.6.1 (Media Format) of the i.MX23 Reference Manual.

0 项奖励
回复
3,311 次查看
Yuri
NXP Employee
NXP Employee

0x80501003 is ERROR_ROM_LDR_SIGNATURE, that means image is not properly flashed.

The image header has incorrect signature.

0x80502008 means  ERROR_ROM_USB_CONNECT_TIMEOUT 

If the boot ROM is unable to boot from the device, indicated by the boot mode

(SD, NAND), then it falls back to the USB interface. This error code indicates

that the USB boot failed as well.