iMX23 SPI USER MODE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX23 SPI USER MODE

2,262 次查看
AndracsEstacvez
Contributor II

Hello everybody,


I'm trying to use SPI from user space. I have already configured the kernel:

<*> User mode SPI device driver support

But I can't see /dev/spidev. Am I missing something?

Regards,

标记 (1)
0 项奖励
回复
3 回复数

1,966 次查看
Balaji_ng
Contributor III

Hi,

Answers inline.

I think that there are some problem because SPI is being used by ethernet. Should it be?

If your target hardware is imx23 evk, you may try loading enc28j60 as module. If you are using spidev, do not load enc28j60.ko module, if you think that is an issue.

Apart from that, I have another problem: I don't have the commands flash_eraseall, ubiattach and ubimkvol. I don't know why. However, I have kobs-ng

I think these are available with mtd-utils package. Try enabling mtd-utils package in ltib configuration. You could refer the following link:

http://processors.wiki.ti.com/index.php/MTD_Utilities#MTD-Utils_User-space_tools

Regards,

Balaji

0 项奖励
回复

1,966 次查看
AndracsEstacvez
Contributor II

Hi Balaji,

thanks for your reply. I think that there are some problem because SPI is being used by ethernet. Should it be?

Apart from that, I have another problem: I don't have the commands flash_eraseall, ubiattach and ubimkvol. I don't know why. However, I have kobs-ng

Thank you,

0 项奖励
回复

1,966 次查看
Balaji_ng
Contributor III

Hi,

It should appear. If not, check if the driver's platform data is defined in the board configuration file for the imx23.

Regards,

Balaji.V

0 项奖励
回复