Hi Nandi,
It appears that the Module needs to be built for specific kernel. Please see if you can get the driver source build inside ltib.
Please place the src files under <ltib_path>/build/rpm folder
The Software is based on the 2.6.31 linux kernel. Installation of the LTIB is essential for driver development.
After LTIB is installed, enter the ltib directory
Configure using "./ltib -m config" from the <ltib> path. Configure parameters and packages as needed.
To Add new packages and Modules, on the <ltib>/config/userspace/packages.lkc add the new Module in Alphabetic order for it to appear in Package list
Second step is to add these packages :
For the <ltib>/config/userspace/ add the section to include a Spec file as listed
ASIX Driver Download Steps to Build on Ubuntu
To build modules under ltib, refer this document Spec file and Module Creation on LTIB
Please let me know if this works. I know that the module you build is wrong. Get it to work on Ubuntu and cross compile later to ARM/Freescale. Sorry cannot any additional thought on how to troubleshoot right now.
HTH,
Vikram U
When I type modprobe mii the following appears:
mii: disagrees about version of symbol netif_carrier_off
mii: Unknown symbol netif_carrier_off
mii: disagrees about version of symbol netif_carrier_onmii: Unknown symbol netif_carrier_on
modprobe: failed to load module mii (/lib/modules/2.6.31-626-g602af1c/kernel/drivers/net/mii.ko): unknown symbol in module, or unknown parameter
The actually module for the ethernet dongle is named asix, but it depends on the mii module:
modprobe asix
and the same errors from modprobe mii appear.
modprobe ehci-hcd (for the usb port) brings up:
fsl-ehci fsl-ehci: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci: irq 11, io base 0x80080000
fsl-ehci fsl-ehci: USB 2.0 started, EHCI 1.00
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
usb 1-1: new high speed USB device using fsl-ehci and address 2
usb 1-1: configuration #1 chosen from 1 choice
lsmod brings up:
Module Size Used by
ehci_hcd 36648 0
lsusb returns nothing
vikram u said:
Hi Nandi,
Could you please post the error log, the lsusb interfaces, details regards the listed modules(lsmod) and help identify why a device is not registered/mounted?.
Hi Nandi,
Could you please post the error log, the lsusb interfaces, details regards the listed modules(lsmod) and help identify why a device is not registered/mounted?.
Hi Nandi,
There are a few USB Dongles available.. closest that might help is the one that works with the chumby board. General pointers are here Chumby USB Ethernet
Hi Nandi,
There are a few USB Dongles available.. closest that might help is the one that works with the chumby board. General pointers are here Chumby USB Ethernet