iMX clock build failed when disable debugfs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX clock build failed when disable debugfs

跳至解决方案
1,962 次查看
xiongweihuang
Contributor III

Hello all

current git source will miss the CONFIG_CLK_DEBUG in arch/arm/plat-mxc/clock.c

Here is the patch file

Please approve

 

Thanks and regards

Original Attachment has been moved to: clock_dbg.patch.zip

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
1,577 次查看
maheshmahadeva1
NXP Employee
NXP Employee

Thanks for the patch. Makes sense, I will push to integrate into the FSL GIT repo.

Best regards,

-Mahesh

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,577 次查看
xiongweihuang
Contributor III

I am glad this is useful

0 项奖励
回复
1,577 次查看
maheshmahadeva1
NXP Employee
NXP Employee

Patch is available on Freescale public GIT at the below link:

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.0.35_4.0.0

0 项奖励
回复
1,578 次查看
maheshmahadeva1
NXP Employee
NXP Employee

Thanks for the patch. Makes sense, I will push to integrate into the FSL GIT repo.

Best regards,

-Mahesh

0 项奖励
回复