iMX clock build failed when disable debugfs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX clock build failed when disable debugfs

ソリューションへジャンプ
1,918件の閲覧回数
xiongweihuang
Contributor III

Hello all

current git source will miss the CONFIG_CLK_DEBUG in arch/arm/plat-mxc/clock.c

Here is the patch file

Please approve

 

Thanks and regards

Original Attachment has been moved to: clock_dbg.patch.zip

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
1,533件の閲覧回数
maheshmahadeva1
NXP Employee
NXP Employee

Thanks for the patch. Makes sense, I will push to integrate into the FSL GIT repo.

Best regards,

-Mahesh

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,533件の閲覧回数
xiongweihuang
Contributor III

I am glad this is useful

0 件の賞賛
返信
1,533件の閲覧回数
maheshmahadeva1
NXP Employee
NXP Employee

Patch is available on Freescale public GIT at the below link:

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.0.35_4.0.0

0 件の賞賛
返信
1,534件の閲覧回数
maheshmahadeva1
NXP Employee
NXP Employee

Thanks for the patch. Makes sense, I will push to integrate into the FSL GIT repo.

Best regards,

-Mahesh

0 件の賞賛
返信