iMX-8ULP HiFi4 On-chip Memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX-8ULP HiFi4 On-chip Memory

241 次查看
caguilar10
Contributor I

Hello,

My understanding is that the HiFi4 in the iMX-8ULP has the following:

- 64KB of ITCM and 64KB of DTCM which I am guessing are zero wait state.

-32KB DCache and 32KB ICache.

Please confirm these numbers. I think it also has an additional amount of on-chip memory that is available for the HiFi4 to use.

Could you confirm what the size of the additional memory and the number of wait states are?

Is this on-chip memory shared with other processors (M33?)?

Thanks

0 项奖励
0 回复数