Hello all,
I have now confirmed the use of i.MX8 Quad Max.
1,
In the datasheet, the LPSPI timing is illustrated with CS active high.

In the reference manual, the default value for CS polarity is active Low.
(CSPOL:00b)

Why is CS shown as active high in the data sheet?
I don't think it is common to use CS in Active High; does NXP's promotion of Active High convey any important message to me?
2,
Where can I get CPHA=1b timing chart?
I want to use it with CPHA=1b but I cannot find its timing chart in the datasheet. I want to check if the characteristics match with my slave device.
CPOL only reverses the polarity of CLK and does not change the timing, but CPHA shifts the phase and therefore changes the timing.
3,
And I cannot discover where to set CPOL and CPHA. At least it is not in the device tree.
Information on the material I am referring to is as follows;
<Datasheet>
i.MX 8QuadMax Industrial Applications Processors
Data Sheet: Technical Data
Document Number: IMX8QMIEC
Rev. 1, 04/2022
<Reference Manual>
i.MX 8QuadMax Applications Processor Reference Manual
Document Number: IMX8QMRM
Rev. 0, 9/2021
Best Regards,
Yukio Oyama