Hello,
I am planning to implement iAP2 support on my iMX6 Nitrogen board, running a Linux 3.0.35. Currently I am struggling with the fact, that the iPhone does not initiate a USB enumeration, and I hope I can get some help here.
What do I currently have:
Of course there are hundreds of possible reasons, and I am trying hard to eliminate one after the other. But for some information I would need a little help:
Currently, I can only imagine that this D+ pin is causing the trouble, since everything else is done as specified. Of course, it can always be a broken phone as well, but I doubt this is the case.
Do you have any information?
Hello,
I'm trying the same with an i.mx 6SoloX Board. I have done the same procedure as you.
As mentioned here: https://www.kernel.org/doc/Documentation/usb/chipidea.txt you can do a roleswitch between two devices from userspace. I have compiled the necessary module into the kernel, but no luck. I see the given files, but when I write to them, nothing changes, no role switch.
In the driver source: Linux/drivers/usb/chipidea/otg.c - Linux Cross Reference - Free Electrons there is a function which does roleswitch depending on the id pin. Perhaps it's possible to turn this off, to make a manual roleswitch?
Regards,
Dennis
Hi Sebastian,
Could u get the solution to your issue.
I am facing the similar issue. Any input would be of great help.
Regards
Zahab
Hi Sebastian
seems some info regarding apple devices one can look at
(USB Role Switch\i.MX6Q\ReleaseNotes.pdf)
How to enable OTG2 to USB device mode in i.MX6 solo lite CPU ? | Freescale Community
Best regards
igor