i2c/adv7180.c vs platform/mxc/capture/adv7180.c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i2c/adv7180.c vs platform/mxc/capture/adv7180.c

509 Views
petero5
Contributor IV

We are using NXP i.MX 8X and ADV7280A-M with MIPI CSI-2 for analog video.
Yocto Scarthgap, Linux 6.6, Qt/QML 6.8.2.

There are two adv7180.c drivers.

i2c/adv7180.c and platform/mxc/capture/adv7180.c

Which of the two drivers is more appropriate in this case?
And why?
Any others we should be aware of?
Should the driver work 100% as is, or are patches needed to get it to work now?
What reference kit is available for i.MX 8X with ADV7280A-M?
Or is there a reference kit with i.MX 8X and another popular analog video ADC?

Thank you
-- Peter

Tags (2)
0 Kudos
Reply
1 Reply

489 Views
joanxie
NXP TechSupport
NXP TechSupport

I think you should use this driver

https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/drivers/media/i2c/adv7180.c

ADV7280 doesn't be tested by imx8qxp, maybe you can refer to this link

https://community.nxp.com/t5/i-MX-Processors/Integrate-ADV7280-M-with-IMX8X/m-p/1633248