i want to use csi2-mipi interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i want to use csi2-mipi interface

525 次查看
srinivas_123
Contributor III

i am using imx8mplus evk . yocto 6.63 BSP version.
i want to use csi2-mipi interface .i am using 0v5640 camera sensor . 

ov5640_1: ov5640_mipi@3c {
compatible = "ovti,ov5640";
reg = <0x3c>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_csi0_pwn>, <&pinctrl_csi0_rst>, <&pinctrl_csi_mclk>;
clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
clock-names = "xclk";
assigned-clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
assigned-clock-parents = <&clk IMX8MP_CLK_24M>;
assigned-clock-rates = <24000000>;
csi_id = <0>;
powerdown-gpios = <&gpio4 1 GPIO_ACTIVE_HIGH>;
reset-gpios = <&gpio4 0 GPIO_ACTIVE_LOW>;
mclk = <24000000>;
mclk_source = <0>;
mipi_csi;
status = "okay";

port {
ov5640_mipi_1_ep: endpoint {
remote-endpoint = <&mipi_csi1_ep>;
data-lanes = <1 2>;
clock-lanes = <0>;
};
};

this is node present in device tree file , I want to use Csi2-mipi interface  , in the above node , csi id is zero , suppose if I want to use csi2-mipi interface , whether I need to write same node with csi id with one . how to approach . 

0 项奖励
回复
1 回复

508 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 项奖励
回复