i am using imx8mplus lpddr4 evk, i build the IMXLXYOCTOUG v.LF6.1.55_2.2.0 bsp version.
how to use the CSI2-MIPI interface.it is not detecting. what are the configurations I have to do?
I am using the ov5640 camera, when I connect this camera to the CSI1-MIPI interface, the camera works.
suppose I connect to the CSI2-MIPI interface, it is not working. what is the reason? if anyone knows please help me out.
Thanks &Regards
Srinivas