i.mx8qm HDMI does not display output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8qm HDMI does not display output

1,662 Views
ruge
Contributor I

nxp工程师,您好。

我是一个嵌入式新手,我想启用imx8qm的HDMI,我做了以下工作:

1.我使用imx_4.14.98_2.0.0_ga/arch/arm64/boot/dts/freescale/fsl-imx8qm-mek-hdmi.dtb这个设备树。

2.我将firmware-imx-8.1-alt1\firmware-imx-8.1\firmware\hdmi\cadence目录下的固件拷贝至/run/media/mmcblk0p1。

3.使用HDMI E Type线缆连接至一个npc mf2203显示器。

我发现显示器插上去毫无反应,就跟HDMI接口没有接任何东西一样。

以下是我的dmesg:

root@imx8qmmek:~# dmesg
[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.14.98 (root@ubuntu) (gcc version 7.3.0 (GCC)) #32 SMP PREEMPT Fri Jun 16 00:47:08 PDT 2023
[    0.000000] Boot CPU: AArch64 Processor [410fd034]
[    0.000000] Machine model: Freescale i.MX8QM MEK
[    0.000000] earlycon: lpuart32 at MMIO 0x000000005a060000 (options '115200')
[    0.000000] bootconsole [lpuart32] enabled
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created CMA memory pool at 0x0000000096000000, size 960 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000090400000, size 28 MiB
[    0.000000] OF: reserved mem: initialized node rpmsg_dma@0x90400000, compatible id shared-dma-pool
[    0.000000] NUMA: No NUMA configuration found
[    0.000000] NUMA: Faking a node at [mem 0x0000000000000000-0x000000097fffffff]
[    0.000000] NUMA: NODE_DATA [mem 0x97ff5f000-0x97ff60dff]
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080200000-0x00000000ffffffff]
[    0.000000]   Normal   [mem 0x0000000100000000-0x000000097fffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080200000-0x0000000083ffffff]
[    0.000000]   node   0: [mem 0x0000000086400000-0x000000008fffffff]
[    0.000000]   node   0: [mem 0x0000000094c00000-0x00000000ffffffff]
[    0.000000]   node   0: [mem 0x0000000880000000-0x000000097fffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080200000-0x000000097fffffff]
[    0.000000] On node 0 totalpages: 1543680
[    0.000000]   DMA zone: 8184 pages used for memmap
[    0.000000]   DMA zone: 0 pages reserved
[    0.000000]   DMA zone: 495104 pages, LIFO batch:31
[    0.000000]   Normal zone: 16384 pages used for memmap
[    0.000000]   Normal zone: 1048576 pages, LIFO batch:31
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.1
[    0.000000] percpu: Embedded 24 pages/cpu @ffff8008ffeca000 s57624 r8192 d32488 u98304
[    0.000000] pcpu-alloc: s57624 r8192 d32488 u98304 alloc=24*4096
[    0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3 [0] 4 [0] 5
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: enabling workaround for ARM erratum 845719
[    0.000000] Speculative Store Bypass Disable mitigation not required
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1519112
[    0.000000] Policy zone: Normal
[    0.000000] Kernel command line: console=ttyLP0,115200 earlycon=lpuart32,0x5a060000,115200 root=/dev/mmcblk0p2 rootwait rw
[    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[    0.000000] software IO TLB: mapped [mem 0xfbfff000-0xfffff000] (64MB)
[    0.000000] Memory: 4871176K/6174720K available (13948K kernel code, 1830K rwdata, 6224K rodata, 1280K init, 435K bss, 320504K reserved, 983040K cma-reserved)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     modules : 0xffff000000000000 - 0xffff000008000000   (   128 MB)
[    0.000000]     vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000   (129022 GB)
[    0.000000]       .text : 0xffff000008080000 - 0xffff000008e20000   ( 13952 KB)
[    0.000000]     .rodata : 0xffff000008e20000 - 0xffff000009440000   (  6272 KB)
[    0.000000]       .init : 0xffff000009440000 - 0xffff000009580000   (  1280 KB)
[    0.000000]       .data : 0xffff000009580000 - 0xffff000009749a00   (  1831 KB)
[    0.000000]        .bss : 0xffff000009749a00 - 0xffff0000097b6958   (   436 KB)
[    0.000000]     fixed   : 0xffff7dfffe7f9000 - 0xffff7dfffec00000   (  4124 KB)
[    0.000000]     PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000   (    16 MB)
[    0.000000]     vmemmap : 0xffff7e0000000000 - 0xffff800000000000   (  2048 GB maximum)
[    0.000000]               0xffff7e0000008000 - 0xffff7e0024000000   (   575 MB actual)
[    0.000000]     memory  : 0xffff800000200000 - 0xffff800900000000   ( 36862 MB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=6, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=6.
[    0.000000]  Tasks RCU enabled.
[    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=6
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: no VLPI support, no direct LPI support
[    0.000000] ITS: No ITS available, not enabling LPIs
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000051b00000
[    0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[    0.000004] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[    0.010937] Console: colour dummy device 80x25
[    0.015086] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[    0.025292] pid_max: default: 32768 minimum: 301
[    0.029960] Security Framework initialized
[    0.036508] Dentry cache hash table entries: 1048576 (order: 11, 8388608 bytes)
[    0.044736] Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes)
[    0.051579] Mount-cache hash table entries: 16384 (order: 5, 131072 bytes)
[    0.058431] Mountpoint-cache hash table entries: 16384 (order: 5, 131072 bytes)
[    0.081747] ASID allocator initialised with 32768 entries
[    0.094833] Hierarchical SRCU implementation.
[    0.107532] *****Initialized MU
[    0.110348] ***** imx8_init_pm_domains *****
[    0.115762] CPU identified as i.MX8QM, silicon rev 1.1
[    0.122083] EFI services will not be available.
[    0.134296] smp: Bringing up secondary CPUs ...
[    0.167143] Detected VIPT I-cache on CPU1
[    0.167172] GICv3: CPU1: found redistributor 1 region 0:0x0000000051b20000
[    0.167202] CPU1: Booted secondary processor [410fd034]
[    0.195157] Detected VIPT I-cache on CPU2
[    0.195172] GICv3: CPU2: found redistributor 2 region 0:0x0000000051b40000
[    0.195187] CPU2: Booted secondary processor [410fd034]
[    0.223204] Detected VIPT I-cache on CPU3
[    0.223219] GICv3: CPU3: found redistributor 3 region 0:0x0000000051b60000
[    0.223233] CPU3: Booted secondary processor [410fd034]
[    0.252250] Detected PIPT I-cache on CPU4
[    0.252268] GICv3: CPU4: found redistributor 100 region 0:0x0000000051b80000
[    0.252285] CPU4: Booted secondary processor [410fd082]
[    0.279290] Detected PIPT I-cache on CPU5
[    0.279301] GICv3: CPU5: found redistributor 101 region 0:0x0000000051ba0000
[    0.279311] CPU5: Booted secondary processor [410fd082]
[    0.279366] smp: Brought up 1 node, 6 CPUs
[    0.363833] SMP: Total of 6 processors activated.
[    0.368522] CPU features: detected feature: GIC system register CPU interface
[    0.375654] CPU features: detected feature: 32-bit EL0 Support
[    0.381464] CPU features: detected feature: Kernel page table isolation (KPTI)
[    0.397505] CPU: All CPU(s) started at EL2
[    0.401279] alternatives: patching kernel code
[    0.406336] devtmpfs: initialized
[    0.421950] random: get_random_u32 called from bucket_table_alloc+0x108/0x260 with crng_init=0
[    0.430759] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.440228] futex hash table entries: 2048 (order: 6, 262144 bytes)
[    0.466869] pinctrl core: initialized pinctrl subsystem
[    0.473841] DMI not present or invalid.
[    0.477655] NET: Registered protocol family 16
[    0.483785] cpuidle: using governor menu
[    0.488580] vdso: 2 pages (1 code @ ffff000008e26000, 1 data @ ffff000009584000)
[    0.495650] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.507271] DMA: preallocated 256 KiB pool for atomic allocations
[    0.513625] Serial: AMBA PL011 UART driver
[    0.517503] imx rpmsg driver is registered.
[    0.523929] MU and Power domains initialized
[    0.527862] ***** imx8qm_clocks_init *****
[    0.594772] imx8qm-pinctrl iomuxc: Invalid fsl,pins or pins property in node /iomuxc/imx8qm-mek/i2c1grp
[    0.603894] imx8qm-pinctrl iomuxc: initialized IMX pinctrl driver
[    0.611795] ARM CCI_400_r1 PMU driver probed
[    0.652011] mxs_phy 5b100000.usbphy: 5b100000.usbphy supply phy-3p0 not found, using dummy regulator
[    0.687823] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.705592] ACPI: Interpreter disabled.
[    0.715886] vgaarb: loaded
[    0.718566] SCSI subsystem initialized
[    0.722142] libata version 3.00 loaded.
[    0.722441] usbcore: registered new interface driver usbfs
[    0.727671] usbcore: registered new interface driver hub
[    0.732955] usbcore: registered new device driver usb
[    0.738629] usb_phy_generic usbphynop1: usbphynop1 supply vcc not found, using dummy regulator
[    0.747240] usb_phy_generic usbphynop2: usbphynop2 supply vcc not found, using dummy regulator
[    0.757256] i2c i2c-4: LPI2C adapter registered
[    0.762158] i2c i2c-5: LPI2C adapter registered
[    0.767010] i2c i2c-6: LPI2C adapter registered
[    0.772143] i2c i2c-7: LPI2C adapter registered
[    0.777492] i2c i2c-8: LPI2C adapter registered
[    0.782525] i2c i2c-9: LPI2C adapter registered
[    0.788203] media: Linux media interface: v0.10
[    0.794171] Linux video capture interface: v2.00
[    0.798563] pps_core: LinuxPPS API ver. 1 registered
[    0.803395] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.812535] PTP clock support registered
[    0.816652] EDAC MC: Ver: 3.0.0
[    0.819797] dmi: Firmware registration failed.
[    0.824825] Advanced Linux Sound Architecture Driver Initialized.
[    0.831092] Bluetooth: Core ver 2.22
[    0.834339] NET: Registered protocol family 31
[    0.838755] Bluetooth: HCI device and connection manager initialized
[    0.845107] Bluetooth: HCI socket layer initialized
[    0.849964] Bluetooth: L2CAP socket layer initialized
[    0.855016] Bluetooth: SCO socket layer initialized
[    0.860614] clocksource: Switched to clocksource arch_sys_counter
[    0.866507] VFS: Disk quotas dquot_6.6.0
[    0.870320] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.877250] pnp: PnP ACPI: disabled
[    0.886120] NET: Registered protocol family 2
[    0.890828] TCP established hash table entries: 65536 (order: 7, 524288 bytes)
[    0.898243] TCP bind hash table entries: 65536 (order: 8, 1048576 bytes)
[    0.905439] TCP: Hash tables configured (established 65536 bind 65536)
[    0.911758] UDP hash table entries: 4096 (order: 5, 131072 bytes)
[    0.917870] UDP-Lite hash table entries: 4096 (order: 5, 131072 bytes)
[    0.924469] NET: Registered protocol family 1
[    0.929138] RPC: Registered named UNIX socket transport module.
[    0.934720] RPC: Registered udp transport module.
[    0.939411] RPC: Registered tcp transport module.
[    0.944098] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.950536] PCI: CLS 0 bytes, default 128
[    0.951915] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[    0.959918] kvm [1]: 8-bit VMID
[    0.964111] kvm [1]: vgic-v2@52020000
[    0.967466] kvm [1]: GIC system register CPU interface enabled
[    0.973355] kvm [1]: vgic interrupt IRQ1
[    0.977284] kvm [1]: Hyp mode initialized successfully
[    0.985003] audit: initializing netlink subsys (disabled)
[    0.990162] audit: type=2000 audit(0.852:1): state=initialized audit_enabled=0 res=1
[    0.990543] workingset: timestamp_bits=44 max_order=21 bucket_order=0
[    1.009332] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    1.015322] NFS: Registering the id_resolver key type
[    1.020053] Key type id_resolver registered
[    1.024201] Key type id_legacy registered
[    1.028258] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    1.034904] jffs2: version 2.2. (NAND) \xc2\xa9 2001-2006 Red Hat, Inc.
[    1.041608] 9p: Installing v9fs 9p2000 file system support
[    1.051029] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[    1.058096] io scheduler noop registered
[    1.062089] io scheduler cfq registered (default)
[    1.066693] io scheduler mq-deadline registered
[    1.071239] io scheduler kyber registered
[    1.094319] OF: PCI: host bridge /pcie@0x5f000000 ranges:
[    1.099391] OF: PCI:   No bus range found for /pcie@0x5f000000, using [bus 00-ff]
[    1.106864] OF: PCI:    IO 0x6ff80000..0x6ff8ffff -> 0x00000000
[    1.112765] OF: PCI:   MEM 0x60000000..0x6fefffff -> 0x60000000
[    1.119904] imx6q-pcie 5f000000.pcie: pcie phy pll is locked.
[    1.370467] imx6q-pcie 5f000000.pcie: phy link never came up
[    1.375800] imx6q-pcie 5f000000.pcie: failed to initialize host
[    1.381701] imx6q-pcie 5f000000.pcie: unable to add pcie port.
[    1.387923] imx6q-pcie: probe of 5f000000.pcie failed with error -110
[    1.395153] pwm-backlight lvds_backlight@0: lvds_backlight@0 supply power not found, using dummy regulator
[    1.405951] pwm-backlight lvds_backlight@1: lvds_backlight@1 supply power not found, using dummy regulator
[    1.423947] Bus freq driver module loaded
[    1.434644] SuperH (H)SCI(F) driver initialized
[    1.439945] msm_serial: driver initialized
[    1.445153] 3b220000.serial: ttyLP5 at MMIO 0x3b220010 (irq = 455, base_baud = 1500000) is a FSL_LPUART
[    1.454581] fsl-lpuart 3b220000.serial: NO DMA tx channel, run at cpu mode
[    1.461130] fsl-lpuart 3b220000.serial: NO DMA rx channel, run at cpu mode
[    1.468660] 5a060000.serial: ttyLP0 at MMIO 0x5a060010 (irq = 66, base_baud = 5000000) is a FSL_LPUART
[    1.479823] console [ttyLP0] enabled
[    1.486810] bootconsole [lpuart32] disabled
[    1.495377] fsl-lpuart 5a060000.serial: NO DMA tx channel, run at cpu mode
[    1.502263] fsl-lpuart 5a060000.serial: NO DMA rx channel, run at cpu mode
[    1.509769] 5a080000.serial: ttyLP2 at MMIO 0x5a080010 (irq = 67, base_baud = 5000000) is a FSL_LPUART
[    1.520093] 5a090000.serial: ttyLP3 at MMIO 0x5a090010 (irq = 68, base_baud = 5000000) is a FSL_LPUART
[    1.529734] fsl-lpuart 5a090000.serial: NO DMA tx channel, run at cpu mode
[    1.536662] fsl-lpuart 5a090000.serial: NO DMA rx channel, run at cpu mode
[    1.546067] arm-smmu 51400000.iommu: probing hardware configuration...
[    1.552613] arm-smmu 51400000.iommu: SMMUv2 with:
[    1.557329] arm-smmu 51400000.iommu:         stage 1 translation
[    1.562732] arm-smmu 51400000.iommu:         stage 2 translation
[    1.568139] arm-smmu 51400000.iommu:         nested translation
[    1.573456] arm-smmu 51400000.iommu:         stream matching with 32 register groups
[    1.580612] arm-smmu 51400000.iommu:         32 context banks (0 stage-2 only)
[    1.587234] Can't support > 32 bit dma.
[    1.591076] arm-smmu 51400000.iommu: failed to set DMA mask for table walker
[    1.598136] arm-smmu 51400000.iommu:         Supported page sizes: 0x61311000
[    1.604671] arm-smmu 51400000.iommu:         Stage-1: 48-bit VA -> 48-bit IPA
[    1.611211] arm-smmu 51400000.iommu:         Stage-2: 48-bit IPA -> 48-bit PA
[    1.664511] imx8-dpr-channel 560d0000.dpr-channel: Linked as a consumer to 56040000.prg
[    1.672830] imx8-dpr-channel 560e0000.dpr-channel: Linked as a consumer to 56050000.prg
[    1.680867] imx8-dpr-channel 560e0000.dpr-channel: Linked as a consumer to 56040000.prg
[    1.689151] imx8-dpr-channel 560f0000.dpr-channel: Linked as a consumer to 56060000.prg
[    1.699454] imx8-dpr-channel 56100000.dpr-channel: Linked as a consumer to 56070000.prg
[    1.707495] imx8-dpr-channel 56100000.dpr-channel: Linked as a consumer to 56080000.prg
[    1.717760] imx8-dpr-channel 56110000.dpr-channel: Linked as a consumer to 56090000.prg
[    1.725802] imx8-dpr-channel 56110000.dpr-channel: Linked as a consumer to 560a0000.prg
[    1.736073] imx8-dpr-channel 56120000.dpr-channel: Linked as a consumer to 560b0000.prg
[    1.744112] imx8-dpr-channel 56120000.dpr-channel: Linked as a consumer to 560c0000.prg
[    1.754456] imx8-dpr-channel 570d0000.dpr-channel: Linked as a consumer to 57040000.prg
[    1.762739] imx8-dpr-channel 570e0000.dpr-channel: Linked as a consumer to 57050000.prg
[    1.770786] imx8-dpr-channel 570e0000.dpr-channel: Linked as a consumer to 57040000.prg
[    1.779077] imx8-dpr-channel 570f0000.dpr-channel: Linked as a consumer to 57060000.prg
[    1.789374] imx8-dpr-channel 57100000.dpr-channel: Linked as a consumer to 57070000.prg
[    1.797415] imx8-dpr-channel 57100000.dpr-channel: Linked as a consumer to 57080000.prg
[    1.807696] imx8-dpr-channel 57110000.dpr-channel: Linked as a consumer to 57090000.prg
[    1.815738] imx8-dpr-channel 57110000.dpr-channel: Linked as a consumer to 570a0000.prg
[    1.826017] imx8-dpr-channel 57120000.dpr-channel: Linked as a consumer to 570b0000.prg
[    1.834057] imx8-dpr-channel 57120000.dpr-channel: Linked as a consumer to 570c0000.prg
[    1.845287] dpu-core 56180000.dpu: Linked as a consumer to 56100000.dpr-channel
[    1.852674] dpu-core 56180000.dpu: Linked as a consumer to 56110000.dpr-channel
[    1.860029] dpu-core 56180000.dpu: Linked as a consumer to 560f0000.dpr-channel
[    1.867410] dpu-core 56180000.dpu: Linked as a consumer to 56120000.dpr-channel
[    1.874745] dpu-core 56180000.dpu: Linked as a consumer to 56020000.pixel-combiner
[    1.883001] dpu-core 56180000.dpu: driver probed
[    1.888583] dpu-core 57180000.dpu: Linked as a consumer to 57100000.dpr-channel
[    1.895970] dpu-core 57180000.dpu: Linked as a consumer to 57110000.dpr-channel
[    1.903321] dpu-core 57180000.dpu: Linked as a consumer to 570f0000.dpr-channel
[    1.910719] dpu-core 57180000.dpu: Linked as a consumer to 57120000.dpr-channel
[    1.918053] dpu-core 57180000.dpu: Linked as a consumer to 57020000.pixel-combiner
[    1.926089] dpu-core 57180000.dpu: driver probed
[    1.934817] imx-drm display-subsystem: parent device of /ldb@562410e0/lvds-channel@0 is not available
[    1.948529] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    1.955168] [drm] No driver support for vblank timestamp query.
[    1.961175] dpu-core 56180000.dpu: Linked as a consumer to 560d0000.dpr-channel
[    1.968519] dpu-core 56180000.dpu: Linked as a consumer to 560e0000.dpr-channel
[    1.975854] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[    1.984010] dpu-core 57180000.dpu: Linked as a consumer to 570d0000.dpr-channel
[    1.991369] dpu-core 57180000.dpu: Linked as a consumer to 570e0000.dpr-channel
[    1.998696] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.5 (ops dpu_bliteng_ops)
[    2.007074] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[    2.014498] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[    2.021935] imx-drm display-subsystem: bound imx-dpu-crtc.3 (ops dpu_crtc_ops)
[    2.029362] imx-drm display-subsystem: bound imx-dpu-crtc.4 (ops dpu_crtc_ops)
[    2.036807] i.mx8-hdp 56268000.hdmi: invalid resource
[    2.041868] i.mx8-hdp 56268000.hdmi: Failed to get HDP RESET base register
[    2.049666] CDN_API_SetClock completed
[    2.053422] [drm] Started firmware!
[    2.056919] [drm] CDN_API_CheckAlive returned ret = 0
[    2.062020] [drm] CDN_API_MainControl_blocking ret = 0 sts = 1
[    2.067947] [drm] CDN_API_General_Test_Echo_Ext_blocking - APB(ret = 0 echo_resp = echo test)
[    2.076486] [drm] CDN_API_General_getCurVersion - ver 26098 verlib 20691
[    2.083206] [drm] phy_cfg_hdp() num_lanes: 4, mode:3840x2160p60, color depth: 8-bit, encoding: 1
[    2.092187] [drm] Pixel clock frequency (594000 kHz) is supported in this color depth (8-bit). Settings found in row 4
[    2.102894] [drm] Character clock frequency: 594000 kHz.
[    2.108217] [drm] VCO frequency (5940000 kHz) is supported. Settings found in row 36
[    2.141201] [drm] CDN_API_General_Write_Register_blocking LANES_CONFIG ret = 0
[    2.148467] [drm] Failed to get HDCP config - using HDCP 2.2 only
[    2.155647] [drm] hdmi-audio-codec driver bound to HDMI
[    2.160886] imx-drm display-subsystem: bound 56268000.hdmi (ops imx_hdp_imx_ops)
[    2.168427] nwl_dsi-imx mipi_dsi@56228000: No bridge found, skipping encoder creation
[    2.176267] imx-drm display-subsystem: bound mipi_dsi@56228000 (ops imx_nwl_dsi_component_ops)
[    2.184965] nwl_dsi-imx mipi_dsi@57228000: No bridge found, skipping encoder creation
[    2.192806] imx-drm display-subsystem: bound mipi_dsi@57228000 (ops imx_nwl_dsi_component_ops)
[    2.201679] /ldb@572410e0/lvds-channel@0: could not find display-timings node
[    2.208824] /ldb@572410e0/lvds-channel@0: no timings specified
[    2.214759] imx-drm display-subsystem: bound ldb@572410e0 (ops imx_ldb_ops)
[    2.301174] Console: switching to colour frame buffer device 128x48
[    2.324078] imx-drm display-subsystem: fb0:  frame buffer device
[    2.330678] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 0
[    2.345342] loop: module loaded
[    2.351104] iommu: Adding device 5f020000.sata to group 0
[    2.358979] ahci-imx 5f020000.sata: phy impedance ratio is not specified.
[    2.366073] ahci-imx 5f020000.sata: internal pll is used.
[    2.374294] ahci-imx 5f020000.sata: no ahb clock.
[    2.379053] Can't support > 32 bit dma.
[    2.382895] ahci-imx 5f020000.sata: Enable 32-bit DMA instead of 64-bit.
[    2.389611] ahci-imx 5f020000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
[    2.398496] ahci-imx 5f020000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sadm sds apst
[    2.409498] scsi host0: ahci-imx
[    2.412877] ata1: SATA max UDMA/133 mmio [mem 0x5f020000-0x5f02ffff] port 0x100 irq 147
[    2.423170] slram: not enough parameters.
[    2.432579] libphy: Fixed MDIO Bus: probed
[    2.437338] NXP PHY: loading NXP PHY driver: [autonomous mode, polling disabled]
[    2.444905] tun: Universal TUN/TAP device driver, 1.6
[    2.450128] CAN device driver interface
[    2.454941] flexcan 5a8d0000.can: 5a8d0000.can supply xceiver not found, using dummy regulator
[    2.464200] flexcan 5a8d0000.can: device registered (reg_base=ffff000010520000, irq=57)
[    2.472830] flexcan 5a8e0000.can: 5a8e0000.can supply xceiver not found, using dummy regulator
[    2.481966] flexcan 5a8e0000.can: device registered (reg_base=ffff000010540000, irq=58)
[    2.492505] iommu: Adding device 5b040000.ethernet to group 1
[    2.499078] fec 5b040000.ethernet: 5b040000.ethernet supply phy not found, using dummy regulator
[    2.507913] fec reset phy !!!!!!!!!!
[    2.511528] fec reset phy 11111!!!!!!!!!!
[    2.515560] fec reset phy 22222!!!!!!!!!!
[    2.519595] fec reset phy 33333!!!!!!!!!!
[    2.523648] fec reset phy 444444!!!!!!!!!!
[    2.734793] ata1: SATA link down (SStatus 0 SControl 300)
[    3.044854] pps pps0: new PPS source ptp0
[    3.049391] fec 5b040000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
[    3.059412] fec 5b040000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 1e:bc:83:49:fe:40
[    3.071509] libphy: fec_enet_mii_bus: probed
[    3.075880] mdio_bus 5b040000.ethernet-1: MDIO device at address 2 is missing.
[    3.083243] mdio_bus 5b040000.ethernet-1: MDIO device at address 4 is missing.
[    3.090552] mdio_bus 5b040000.ethernet-1: MDIO device at address 5 is missing.
[    3.098229] fec 5b040000.ethernet eth0: registered PHC device 0
[    3.104787] iommu: Adding device 5b050000.ethernet to group 1
[    3.111941] imx8qm-pinctrl iomuxc: pin SC_P_COMP_CTL_GPIO_1V8_3V3_ENET_ENETA already requested by 5b050000.ethernet; cannot claim for fixed-0:00
[    3.124939] imx8qm-pinctrl iomuxc: pin-268 (fixed-0:00) status -22
[    3.131150] imx8qm-pinctrl iomuxc: could not request pin 268 (SC_P_COMP_CTL_GPIO_1V8_3V3_ENET_ENETA) from group fec2grp  on device iomuxc
[    3.143508] TJA1102_p1 fixed-0:00: Error applying setting, reverse things back
[    3.150769] TJA1102_p1: probe of fixed-0:00 failed with error -22
[    3.157152] fec reset phy !!!!!!!!!!
[    3.160764] fec reset phy 11111!!!!!!!!!!
[    3.165009] pps pps1: new PPS source ptp1
[    3.169535] fec 5b050000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
[    3.179561] fec 5b050000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: b6:e6:32:3a:e0:ec
[    3.191644] libphy: fec_enet_mii_bus: probed
[    3.196183] /****************************tja110x_probe*****************/
[    3.202912] TJA1102_p0 5b050000.ethernet-2:08: probing PHY 8
[    3.208682] TJA1102_p0 5b050000.ethernet-2:08: Could not retrieve GPIO from device tree
[    3.216717] TJA1102_p0 5b050000.ethernet-2:08: Ignoring interrupts
[    3.223177] /****************************tja110x_probe*****************/
[    3.229916] TJA1102_p1 5b050000.ethernet-2:09: probing PHY 9
[    3.235619] TJA1102_p1 5b050000.ethernet-2:09: Could not retrieve GPIO from device tree
[    3.243639] TJA1102_p1 5b050000.ethernet-2:09: Ignoring interrupts
[    3.249960] mdio_bus 5b050000.ethernet-2: MDIO device at address 2 is missing.
[    3.257265] mdio_bus 5b050000.ethernet-2: MDIO device at address 3 is missing.
[    3.264946] fec 5b050000.ethernet eth1: registered PHC device 1
[    3.271959] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[    3.277806] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[    3.283798] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.4.0-k
[    3.290779] igb: Copyright (c) 2007-2014 Intel Corporation.
[    3.296390] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[    3.304249] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    3.310757] sky2: driver version 1.30
[    3.315038] PPP generic driver version 2.4.2
[    3.319435] PPP BSD Compression module registered
[    3.324156] PPP Deflate Compression module registered
[    3.329257] PPP MPPE Compression module registered
[    3.334074] NET: Registered protocol family 24
[    3.338629] usbcore: registered new interface driver cdc_ether
[    3.344506] usbcore: registered new interface driver net1080
[    3.350235] usbcore: registered new interface driver rndis_host
[    3.356195] usbcore: registered new interface driver cdc_subset
[    3.362150] usbcore: registered new interface driver zaurus
[    3.367785] usbcore: registered new interface driver cdc_ncm
[    3.379872] Can't support > 32 bit dma.
[    3.383756]  xhci-cdns3: xHCI Host Controller
[    3.388134]  xhci-cdns3: new USB bus registered, assigned bus number 1
[    3.419747]  xhci-cdns3: hcc params 0x200073c8 hci version 0x100 quirks 0xffffffffa0010010
[    3.428582] hub 1-0:1.0: USB hub found
[    3.432378] hub 1-0:1.0: 1 port detected
[    3.436539]  xhci-cdns3: xHCI Host Controller
[    3.440909]  xhci-cdns3: new USB bus registered, assigned bus number 2
[    3.447467]  xhci-cdns3: Host supports USB 3.0  SuperSpeed
[    3.453004] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[    3.461456] hub 2-0:1.0: USB hub found
[    3.465245] hub 2-0:1.0: 1 port detected
[    3.469613] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    3.476147] ehci-pci: EHCI PCI platform driver
[    3.480715] ehci-platform: EHCI generic platform driver
[    3.486497] ehci-orion: EHCI orion driver
[    3.490716] ehci-exynos: EHCI EXYNOS driver
[    3.495076] ehci-msm: Qualcomm On-Chip EHCI Host Controller
[    3.500826] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[    3.507027] ohci-pci: OHCI PCI platform driver
[    3.511530] ohci-platform: OHCI generic platform driver
[    3.516979] ohci-exynos: OHCI EXYNOS driver
[    3.522034] usbcore: registered new interface driver usb-storage
[    3.528122] usbcore: registered new interface driver usbserial
[    3.534013] usbcore: registered new interface driver usbserial_generic
[    3.540572] usbserial: USB Serial support registered for generic
[    3.546640] usbcore: registered new interface driver ftdi_sio
[    3.552416] usbserial: USB Serial support registered for FTDI USB Serial Device
[    3.559821] usbcore: registered new interface driver option
[    3.565443] usbserial: USB Serial support registered for GSM modem (1-port)
[    3.572518] usbcore: registered new interface driver pl2303
[    3.578118] usbserial: USB Serial support registered for pl2303
[    3.584099] usbcore: registered new interface driver usb_ehset_test
[    3.592205] usbmisc_imx 5b0d0200.usbmisc: 5b0d0200.usbmisc supply vbus-wakeup not found, using dummy regulator
[    3.602695] usbmisc_imx 5b0e0200.usbmisc: 5b0e0200.usbmisc supply vbus-wakeup not found, using dummy regulator
[    3.614041] imx_usb 5b0d0000.usb: 5b0d0000.usb supply vbus not found, using dummy regulator
[    3.627491] ci_hdrc ci_hdrc.0: EHCI Host Controller
[    3.632437] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 3
[    3.656630] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[    3.662538] hub 3-0:1.0: USB hub found
[    3.666314] hub 3-0:1.0: 1 port detected
[    3.673180] input: sc-powerkey as /devices/platform/sc-powerkey/input/input0
[    3.682436] imx_sc_rtc rtc: rtc core: registered rtc as rtc0
[    3.688571] i2c /dev entries driver
[    3.695125] IR NEC protocol handler initialized
[    3.699667] IR RC5(x/sz) protocol handler initialized
[    3.704725] IR RC6 protocol handler initialized
[    3.709265] IR JVC protocol handler initialized
[    3.713799] IR Sony protocol handler initialized
[    3.718421] IR SANYO protocol handler initialized
[    3.723129] IR Sharp protocol handler initialized
[    3.727838] IR MCE Keyboard/mouse protocol handler initialized
[    3.733676] IR XMP protocol handler initialized
[    3.745420] mxc-mipi-csi2 58227000.csi: mipi_csi2_probe
[    3.769532] mxc-mipi-csi2 58247000.csi: mipi_csi2_probe
[    3.784631] usb 1-1: new high-speed USB device number 2 using cdns-usb3
[    3.794306] ___lp___enter max9286_probe 1 time___
[    3.799069] ______________max9286_hw_reset________________
[    3.938863] hub 1-1:1.0: USB hub found
[    3.948169] hub 1-1:1.0: 4 ports detected
[    3.965128] ___lp___max9286_probe___006___
[    3.969235] max9286_mipi 8-006a: In max9286_hardware_preinit()
[    4.477103] max9286_mipi: reg = 0x00.
[    4.480784] max9286_mipi: sensor number = 0.
[    4.485059] max9286_hardware_preinit: no camera connected.
[    4.490549] cameras are not found,
[    4.494977] ___lp___enter max9286_probe 2 time___
[    4.499764] ______________max9286_hw_reset________________
[    4.665105] ___lp___max9286_probe___006___
[    4.674700] max9286_mipi 9-006a: In max9286_hardware_preinit()
[    5.185105] max9286_mipi: reg = 0x00.
[    5.188772] max9286_mipi: sensor number = 0.
[    5.193048] max9286_hardware_preinit: no camera connected.
[    5.198552] cameras are not found,
[    5.203217] mx8-img-md: Registered mxc_isi.0.capture as /dev/video0
[    5.209598] mx8-img-md: Registered mxc_isi.1.capture as /dev/video1
[    5.215994] mx8-img-md: Registered mxc_isi.2.capture as /dev/video2
[    5.222390] mx8-img-md: Registered mxc_isi.3.capture as /dev/video3
[    5.228768] mx8-img-md: Registered mxc_isi.4.capture as /dev/video4
[    5.235163] mx8-img-md: Registered mxc_isi.5.capture as /dev/video5
[    5.241534] mx8-img-md: Registered mxc_isi.6.capture as /dev/video6
[    5.247929] mx8-img-md: Registered mxc_isi.7.capture as /dev/video7
[    5.254290] mxc-isi 58170000.isi: register m2m device success
[    5.260287] mxc-isi 58100000.isi: mxc_md_unregister_all unregister ISI channel[0]
[    5.267869] mxc-isi 58110000.isi: mxc_md_unregister_all unregister ISI channel[1]
[    5.275433] mxc-isi 58120000.isi: mxc_md_unregister_all unregister ISI channel[2]
[    5.283009] mxc-isi 58130000.isi: mxc_md_unregister_all unregister ISI channel[3]
[    5.290567] mxc-isi 58140000.isi: mxc_md_unregister_all unregister ISI channel[4]
[    5.298143] mxc-isi 58150000.isi: mxc_md_unregister_all unregister ISI channel[5]
[    5.305706] mxc-isi 58160000.isi: mxc_md_unregister_all unregister ISI channel[6]
[    5.313282] mxc-isi 58170000.isi: mxc_md_unregister_all unregister ISI channel[7]
[    5.322144] mxc-jpeg 58400000.jpegdec: decoder device registered as /dev/video0 (81,0)
[    5.330985] mxc-jpeg 58450000.jpegenc: encoder device registered as /dev/video1 (81,1)
[    5.345468] Bluetooth: HCI UART driver ver 2.3
[    5.349957] Bluetooth: HCI UART protocol H4 registered
[    5.355103] Bluetooth: HCI UART protocol BCSP registered
[    5.360420] Bluetooth: HCI UART protocol ATH3K registered
[    5.365841] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    5.372228] Bluetooth: HCI UART protocol Broadcom registered
[    5.377892] Bluetooth: HCI UART protocol QCA registered
[    5.384077] sdhci: Secure Digital Host Controller Interface driver
[    5.390266] sdhci: Copyright(c) Pierre Ossman
[    5.394929] Synopsys Designware Multimedia Card Interface Driver
[    5.402494] sdhci-pltfm: SDHCI platform and OF driver helper
[    5.409704] iommu: Adding device 5b010000.usdhc to group 2
[    5.460661] mmc0: SDHCI controller on 5b010000.usdhc [5b010000.usdhc] using ADMA
[    5.472905] sdhci-esdhc-imx 5b030000.usdhc: assigned as wifi host
[    5.476152] random: fast init done
[    5.528647] mmc2: SDHCI controller on 5b030000.usdhc [5b030000.usdhc] using ADMA
[    5.543604] mxc_mlb150 5b060000.mlb: 5b060000.mlb supply reg_nvcc not found, using dummy regulator
[    5.550162] mmc0: new HS400 MMC card at address 0001
[    5.552652] mxc_mlb150 5b060000.mlb: enalbe regulator
[    5.558230] mmcblk0: mmc0:0001 S0J57X 29.6 GiB
[    5.562699] mxc_mlb150 5b060000.mlb: no iram assigned, using external mem
[    5.567630] mmcblk0boot0: mmc0:0001 S0J57X partition 1 31.5 MiB
[    5.580370] mmcblk0boot1: mmc0:0001 S0J57X partition 2 31.5 MiB
[    5.582220] Galcore version 6.2.4.190076
[    5.586776] mmcblk0rpmb: mmc0:0001 S0J57X partition 3 4.00 MiB
[    5.599653]  mmcblk0: p1 p2 p3 p4 p5
[    5.774880] ledtrig-cpu: registered to indicate activity on CPUs
[    5.785034] caam 31400000.caam: ERA source: device tree.
[    5.800498] caam algorithms registered in /proc/crypto
[    5.808203] caam_jr 31430000.jr2: registering rng-caam
[    5.813692] caam 31400000.caam: caam pkc algorithms registered in /proc/crypto
[    5.822999] platform caam_sm: blkkey_ex: 8 keystore units available
[    5.829375] platform caam_sm: 64-bit clear key:
[    5.833954] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[    5.839627] platform caam_sm: 64-bit black key:
[    5.844172] platform caam_sm: [0000] 63 37 6e d3 8c 68 23 14
[    5.849859] platform caam_sm: [0008] 30 6a 43 19 e8 ff 4d 02
[    5.855521] platform caam_sm: 128-bit clear key:
[    5.860144] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[    5.865829] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[    5.871498] platform caam_sm: 128-bit black key:
[    5.876127] platform caam_sm: [0000] d6 7e c7 20 a3 f3 fb 46
[    5.881811] platform caam_sm: [0008] fe aa 06 f1 e8 75 c2 97
[    5.887475] platform caam_sm: 192-bit clear key:
[    5.892098] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[    5.897779] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[    5.903444] platform caam_sm: [0016] 10 11 12 13 14 15 16 17
[    5.909105] platform caam_sm: 192-bit black key:
[    5.913745] platform caam_sm: [0000] f1 33 f0 03 ce 75 e5 3e
[    5.919412] platform caam_sm: [0008] 6d 20 98 6e 37 68 3d 58
[    5.925076] platform caam_sm: [0016] ea fb ad 88 12 77 9f d6
[    5.930755] platform caam_sm: [0024] fe 76 f0 1e 3a 7b cd 62
[    5.936420] platform caam_sm: 256-bit clear key:
[    5.941043] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[    5.946723] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[    5.952392] platform caam_sm: [0016] 10 11 12 13 14 15 16 17
[    5.958093] platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
[    5.963776] platform caam_sm: 256-bit black key:
[    5.968401] platform caam_sm: [0000] ee 93 93 ed cd ff 83 5b
[    5.974064] platform caam_sm: [0008] d4 75 47 34 ba b6 3f c2
[    5.979744] platform caam_sm: [0016] 6b db 55 b1 55 21 1c 59
[    5.985411] platform caam_sm: [0024] b1 e2 68 8b 49 cb 3b b6
[    5.991072] platform caam_sm: 64-bit unwritten blob:
[    5.996046] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[    6.001733] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[    6.007398] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[    6.013079] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[    6.018744] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[    6.024408] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[    6.030088] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[    6.035757] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[    6.041428] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[    6.047108] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[    6.052773] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[    6.058440] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[    6.064125] platform caam_sm: 128-bit unwritten blob:
[    6.069184] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[    6.074847] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[    6.080529] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[    6.086194] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[    6.091857] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[    6.097539] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[    6.103204] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[    6.108869] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[    6.114548] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[    6.120217] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[    6.125887] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[    6.131568] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[    6.137232] platform caam_sm: 196-bit unwritten blob:
[    6.142288] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[    6.147969] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[    6.153635] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[    6.159298] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[    6.164980] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[    6.170645] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[    6.176308] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[    6.181991] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[    6.187656] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[    6.193319] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[    6.198999] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[    6.204664] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[    6.210327] platform caam_sm: 256-bit unwritten blob:
[    6.215402] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[    6.221066] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[    6.226731] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[    6.232412] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[    6.238077] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[    6.243741] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[    6.249432] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[    6.255096] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[    6.260761] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[    6.266441] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[    6.272105] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[    6.277771] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[    6.283531] platform caam_sm: 64-bit black key in blob:
[    6.288764] platform caam_sm: [0000] ad b0 60 fe 6d 9f 0a d0
[    6.294434] platform caam_sm: [0008] b0 8a 71 8f 0f dc 01 e7
[    6.300115] platform caam_sm: [0016] e0 66 ce 20 80 0b af d8
[    6.305780] platform caam_sm: [0024] 53 c2 3a 23 e5 cf de 25
[    6.311443] platform caam_sm: [0032] 5c b3 10 2b f1 51 6f f7
[    6.317127] platform caam_sm: [0040] ed ee 79 14 54 b1 45 49
[    6.322799] platform caam_sm: [0048] f0 01 78 a7 d6 11 5a 7f
[    6.328462] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[    6.334142] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[    6.339808] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[    6.345472] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[    6.351161] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[    6.356827] platform caam_sm: 128-bit black key in blob:
[    6.362146] platform caam_sm: [0000] 43 9b 28 70 59 73 e4 46
[    6.367832] platform caam_sm: [0008] 44 15 b1 f8 5d 1b a6 fa
[    6.373503] platform caam_sm: [0016] 5d 1b 82 f1 10 95 d5 f3
[    6.379171] platform caam_sm: [0024] d6 cd cd 77 7c 98 1a dd
[    6.384853] platform caam_sm: [0032] ce 61 a0 43 11 88 b9 41
[    6.390517] platform caam_sm: [0040] b0 7f f5 91 e9 f7 ae e1
[    6.396181] platform caam_sm: [0048] 8e 7c 50 50 c3 2f b4 3d
[    6.401871] platform caam_sm: [0056] fd b6 a7 af 3c 64 cc 5a
[    6.407536] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[    6.413215] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[    6.418882] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[    6.424545] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[    6.430227] platform caam_sm: 192-bit black key in blob:
[    6.435545] platform caam_sm: [0000] e4 ad 1a eb 9b 00 e1 d6
[    6.441209] platform caam_sm: [0008] d8 a6 d6 9a 09 54 7e 19
[    6.446890] platform caam_sm: [0016] 33 b5 3a bc 81 97 a0 50
[    6.452554] platform caam_sm: [0024] 43 1f 88 8d b4 1f f9 f7
[    6.458222] platform caam_sm: [0032] b7 7a 49 8a 66 55 2b b6
[    6.463910] platform caam_sm: [0040] 8e 2f bc 19 d7 d5 b2 b4
[    6.469574] platform caam_sm: [0048] de d7 bf 8f 13 84 49 f5
[    6.475237] platform caam_sm: [0056] 1b ae 23 63 b5 3c 01 be
[    6.480919] platform caam_sm: [0064] d1 b4 e7 f2 fa 04 80 8d
[    6.486583] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[    6.492246] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[    6.497928] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[    6.503591] platform caam_sm: 256-bit black key in blob:
[    6.508910] platform caam_sm: [0000] f6 9a 09 3f 19 87 08 15
[    6.514591] platform caam_sm: [0008] 28 2e c5 c5 c7 a6 bf c4
[    6.520256] platform caam_sm: [0016] 8b 78 e4 f5 43 d6 4b 20
[    6.525919] platform caam_sm: [0024] 6c 51 8f b9 77 3b 47 6e
[    6.531601] platform caam_sm: [0032] d0 50 06 2c bf be 35 f6
[    6.537270] platform caam_sm: [0040] 9f 08 d5 ef df 2d b3 3a
[    6.542938] platform caam_sm: [0048] 6e da cd 1c bc 4d 31 e1
[    6.548640] platform caam_sm: [0056] c8 7f 3f 24 ce bd 1f 46
[    6.554312] platform caam_sm: [0064] 8a 64 1f 0f bd 38 34 67
[    6.559975] platform caam_sm: [0072] f5 1f 38 07 cb a3 e9 52
[    6.565658] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[    6.571323] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[    6.577074] platform caam_sm: restored 64-bit black key:
[    6.582415] platform caam_sm: [0000] 33 19 86 6c e5 32 1a 1f
[    6.588081] platform caam_sm: [0008] 06 ab 78 d6 be 27 c1 ec
[    6.593751] platform caam_sm: restored 128-bit black key:
[    6.599173] platform caam_sm: [0000] d6 7e c7 20 a3 f3 fb 46
[    6.604837] platform caam_sm: [0008] fe aa 06 f1 e8 75 c2 97
[    6.610500] platform caam_sm: restored 192-bit black key:
[    6.615922] platform caam_sm: [0000] f1 33 f0 03 ce 75 e5 3e
[    6.621587] platform caam_sm: [0008] 6d 20 98 6e 37 68 3d 58
[    6.627252] platform caam_sm: [0016] a7 1e bd b3 27 51 05 26
[    6.632932] platform caam_sm: [0024] 76 aa aa a0 73 3c c8 d7
[    6.638594] platform caam_sm: restored 256-bit black key:
[    6.644001] platform caam_sm: [0000] ee 93 93 ed cd ff 83 5b
[    6.649681] platform caam_sm: [0008] d4 75 47 34 ba b6 3f c2
[    6.655346] platform caam_sm: [0016] 6b db 55 b1 55 21 1c 59
[    6.661011] platform caam_sm: [0024] b1 e2 68 8b 49 cb 3b b6
[    6.667670] usbcore: registered new interface driver usbhid
[    6.673253] usbhid: USB HID core driver
[    6.685503] rt5640 i2c probe !!!!!!!
[    6.689319] rt5640 6-001c: Device with ID register 0xffff0000 is not rt5640/39
[    6.698305] ***** imx8qm_acm_init *****
[    6.734621] imx-rt5640 sound: failed to find codec platform device
[    6.740832] imx-rt5640: probe of sound failed with error -22
[    6.751102] imx-spdif sound-hdmi-arc: snd-soc-dummy-dai <-> 59030000.spdif mapping ok
[    6.758978] imx-spdif sound-hdmi-arc: ASoC: no DMI vendor name!
[    6.768499] imx-cdnhdmi sound-hdmi-tx: i2s-hifi <-> 59090000.sai mapping ok
[    6.775505] imx-cdnhdmi sound-hdmi-tx: ASoC: no DMI vendor name!
[    6.782532] NET: Registered protocol family 26
[    6.787420] nf_conntrack version 0.5.0 (65536 buckets, 262144 max)
[    6.794051] ip_tables: (C) 2000-2006 Netfilter Core Team
[    6.800088] NET: Registered protocol family 10
[    6.805246] Segment Routing with IPv6
[    6.808951] NET: Registered protocol family 17
[    6.813430] can: controller area network core (rev 20170425 abi 9)
[    6.819655] NET: Registered protocol family 29
[    6.824121] can: raw protocol (rev 20170425)
[    6.828400] can: broadcast manager protocol (rev 20170425 t)
[    6.834092] can: netlink gateway (rev 20170425) max_hops=1
[    6.839715] Bluetooth: RFCOMM TTY layer initialized
[    6.844628] Bluetooth: RFCOMM socket layer initialized
[    6.849799] Bluetooth: RFCOMM ver 1.11
[    6.853557] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    6.858875] Bluetooth: BNEP filters: protocol multicast
[    6.864128] Bluetooth: BNEP socket layer initialized
[    6.869102] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    6.875030] Bluetooth: HIDP socket layer initialized
[    6.880064] lib80211: common routines for IEEE802.11 drivers
[    6.885732] lib80211_crypt: registered algorithm 'NULL'
[    6.885735] lib80211_crypt: registered algorithm 'WEP'
[    6.885738] lib80211_crypt: registered algorithm 'CCMP'
[    6.885740] lib80211_crypt: registered algorithm 'TKIP'
[    6.885762] 9pnet: Installing 9P2000 support
[    6.890084] Key type dns_resolver registered
[    6.894900] registered taskstats version 1
[    6.919428] imx8_cpufreq_init: cluster 0 running at freq 1200 MHz, suspend freq 1200 MHz
[    6.927916] imx8_cpufreq_init: cluster 1 running at freq 1596 MHz, suspend freq 1596 MHz
[    6.941082] imx_sc_rtc rtc: setting system clock to 1970-01-01 00:00:11 UTC (11)
[    6.951786] sw-3p3-sd1: disabling
[    6.955113] vref_1v8: disabling
[    6.958261] ALSA device list:
[    6.961230]   #0: imx-hdmi-arc
[    6.964282]   #1: imx-audio-hdmi-tx
[    6.976154] EXT4-fs (mmcblk0p2): mounting ext3 file system using the ext4 subsystem
[    7.047330] EXT4-fs (mmcblk0p2): recovery complete
[    7.053299] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    7.061650] VFS: Mounted root (ext3 filesystem) on device 179:2.
[    7.069389] devtmpfs: mounted
[    7.072995] Freeing unused kernel memory: 1280K
[    7.147763] systemd[1]: System time before build time, advancing clock.
[    7.164084] systemd[1]: systemd 237 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[    7.185979] systemd[1]: Detected architecture arm64.
[    7.204920] systemd[1]: Set hostname to <imx8qmmek>.
[    7.265501] systemd-gpt-auto-generator[2332]: Failed to dissect: Input/output error
[    7.273726] systemd[2327]: /lib/systemd/system-generators/systemd-gpt-auto-generator failed with exit status 1.
[    7.293678] systemd[1]: File /lib/systemd/system/systemd-journald.service:35 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
[    7.310755] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
[    7.389293] systemd[1]: Configuration file /lib/systemd/system/startserver.service is marked executable. Please remove executable permission bits. Proceeding anyway.
[    7.408457] random: systemd: uninitialized urandom read (16 bytes read)
[    7.415312] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[    7.440754] random: systemd: uninitialized urandom read (16 bytes read)
[    7.448494] systemd[1]: Created slice User and Session Slice.
[    7.464762] random: systemd: uninitialized urandom read (16 bytes read)
[    7.472012] systemd[1]: Created slice System Slice.
[    7.720444] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[    8.170298] systemd-journald[2352]: Received request to flush runtime journal from PID 1
[    8.228326] [VPU Encoder]     enable mu for core[0]
[    8.240552] [VPU Encoder]     vpu encoder core[0] firmware version is 1.2.6
[    8.404098] Generic PHY fixed-0:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=fixed-0:00, irq=POLL)
[    8.415124] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[    8.595184] EXT4-fs (mmcblk0p5): mounting ext3 file system using the ext4 subsystem
[    8.605431] EXT4-fs (mmcblk0p3): mounting ext3 file system using the ext4 subsystem
[    8.608383] EXT4-fs (mmcblk0p5): recovery complete
[    8.616002] FAT-fs (mmcblk0p4): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[    8.617972] EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: (null)
[    8.628180] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[    8.632952] EXT4-fs (mmcblk0p3): recovery complete
[    8.632961] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)
[    9.130283] sja1105pqrs: loading out-of-tree module taints kernel.
[    9.138861] sja1105pqrs spi0.0: Loading SJA1105P SPI driver
[    9.144731] sja1105pqrs spi0.0: Probing switch number 0
[    9.144736] sja1105pqrs spi0.0: SJA1105P SPI Clock set to 25000000Hz, bits per word set to 32
[    9.144751] sja1105pqrs spi0.0: Found a matching DT entry (type 0)
[    9.144755] sja1105pqrs spi0.0: [Roy_test ] sja1105p_probe 712
[    9.144760] sja1105pqrs spi0.0: [Roy_test ] sja1105p_probe 719
[    9.144765] sja1105pqrs spi0.0: Firmware name "sja1105p-1_cfg.bin" found
[    9.144771] sja1105pqrs spi0.0: Properties of port 0 found
[    9.144777] sja1105pqrs spi0.0: port-0 logical-port-num=0
[    9.144781] sja1105pqrs spi0.0: port-0 is-host=1
[    9.144786] sja1105pqrs spi0.0: port-0 null-phy=1 (phy_not_mac=1)
[    9.144790] sja1105pqrs spi0.0: No rx-delay declared in dtb for host port
[    9.144793] sja1105pqrs spi0.0: No tx-delay declared in dtb for host port
[    9.144797] sja1105pqrs spi0.0: Properties of port 1 found
[    9.144802] sja1105pqrs spi0.0: port-1 logical-port-num=1
[    9.144809] sja1105pqrs spi0.0: port-1 is-host=0
[    9.234122] sja1105pqrs spi0.0: port-1 null-phy=0 (phy_not_mac=0)
[    9.240244] sja1105pqrs spi0.0: Properties of port 2 found
[    9.240249] sja1105pqrs spi0.0: port-2 logical-port-num=2
[    9.240253] sja1105pqrs spi0.0: port-2 is-host=0
[    9.240258] sja1105pqrs spi0.0: port-2 null-phy=0 (phy_not_mac=0)
[    9.240263] sja1105pqrs spi0.0: Properties of port 3 found
[    9.240267] sja1105pqrs spi0.0: port-3 logical-port-num=3
[    9.240271] sja1105pqrs spi0.0: port-3 is-host=0
[    9.240275] sja1105pqrs spi0.0: port-3 null-phy=0 (phy_not_mac=0)
[    9.240281] sja1105pqrs spi0.0: Properties of port 4 found
[    9.240285] sja1105pqrs spi0.0: port-4 logical-port-num=4
[    9.240289] sja1105pqrs spi0.0: port-4 is-host=0
[    9.240293] sja1105pqrs spi0.0: port-4 null-phy=0 (phy_not_mac=0)
[    9.240306] sja1105pqrs spi0.0: [Roy_test ] sja1105p_probe 726
[    9.240437] sja1105pqrs spi0.0: Detected Device ID ae00030e ()
[    9.240884] sja1105pqrs spi0.0: SJA1105P switch preparing to load sja1105p-1_cfg.bin
[    9.333855] sja1105pqrs spi0.0: SJA1105P switch firmware request succeeded
[    9.343141] sja1105pqrs spi0.0: REG_PORT_STATUS(0): speed=2 phyMode=1 xmiiMode=3
[    9.350692] sja1105pqrs spi0.0: REG_PORT_STATUS(1): speed=2 phyMode=1 xmiiMode=3
[    9.358292] sja1105pqrs spi0.0: REG_PORT_STATUS(2): speed=2 phyMode=1 xmiiMode=3
[    9.365900] sja1105pqrs spi0.0: REG_PORT_STATUS(3): speed=2 phyMode=1 xmiiMode=3
[    9.373581] sja1105pqrs spi0.0: REG_PORT_STATUS(4): speed=2 phyMode=1 xmiiMode=3
[    9.381153] sja1105pqrs spi0.0: Config 1st word=ae00030e
[    9.386535] sja1105pqrs spi0.0: Config Block Id=0x5 size=5 CRC=9a1ca02b offset=1 total_size=9
[    9.395150] sja1105pqrs spi0.0: Config Block Id=0x6 size=90 CRC=4ed2c50f offset=10 total_size=103
[    9.404097] sja1105pqrs spi0.0: Config Block Id=0x7 size=34 CRC=dd3964cc offset=104 total_size=141
[    9.413113] sja1105pqrs spi0.0: Config Block Id=0x8 size=26 CRC=6af62353 offset=142 total_size=171
[    9.422134] sja1105pqrs spi0.0: Config Block Id=0x9 size=40 CRC=db43ac9 offset=172 total_size=215
[    9.431070] sja1105pqrs spi0.0: Config Block Id=0xd size=4 CRC=12d08c8f offset=216 total_size=223
[    9.439995] sja1105pqrs spi0.0: Config Block Id=0xe size=3 CRC=c8a7cee6 offset=224 total_size=230
[    9.445973] fec 5b050000.ethernet eth1: Link is Up - 1Gbps/Full - flow control off
[    9.448917] sja1105pqrs spi0.0: Config Block Id=0x10 size=4 CRC=8aa0dfbc offset=231 total_size=238
[    9.456495] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready
[    9.465495] sja1105pqrs spi0.0: Config Block Id=0x11 size=11 CRC=efa3e65a offset=239 total_size=253
[    9.480804] sja1105pqrs spi0.0: Config Block Id=0x4e size=1 CRC=3a5d5e24 offset=254 total_size=258
[    9.489803] sja1105pqrs spi0.0: Config Block Id=0x0 size=0 CRC=4d37fb9f offset=259 total_size=262
[    9.489810] sja1105pqrs spi0.0: Final Block
[    9.502890] sja1105pqrs spi0.0: Looking for AVB parameters
[    9.508412] sja1105pqrs spi0.0: Got dev=ffff8008f7e5e000 name= eth0
[    9.514699] sja1105pqrs spi0.0: Registered management port DST MAC address=f0:0d:98:80:b7:b2
[    9.524694] sja1105pqrs spi0.0: Registered management port SRC MAC address=00:00:00:80:fb:3f
[    9.533152] sja1105pqrs spi0.0: swap_required 0 nb_words 262 dev_addr 00020000
[    9.543379] sja1105pqrs spi0.0: REG_PORT_STATUS(0): speed=2 phyMode=0 xmiiMode=2
[    9.550896] sja1105pqrs spi0.0: REG_PORT_STATUS(1): speed=1 phyMode=0 xmiiMode=0
[    9.558435] sja1105pqrs spi0.0: REG_PORT_STATUS(2): speed=1 phyMode=0 xmiiMode=0
[    9.565927] sja1105pqrs spi0.0: REG_PORT_STATUS(3): speed=1 phyMode=0 xmiiMode=2
[    9.573396] sja1105pqrs spi0.0: REG_PORT_STATUS(4): speed=1 phyMode=0 xmiiMode=2
[    9.580808] sja1105pqrs spi0.0: SJA1105P (number 0) successfully configured!
[    9.587888] sja1105pqrs spi0.0: physical-port-0: logical-port-0, switch-0
[    9.594741] sja1105pqrs spi0.0: physical-port-1: logical-port-1, switch-0
[    9.601553] sja1105pqrs spi0.0: physical-port-2: logical-port-2, switch-0
[    9.608402] sja1105pqrs spi0.0: physical-port-3: logical-port-3, switch-0
[    9.615235] sja1105pqrs spi0.0: physical-port-4: logical-port-4, switch-0
[    9.622164] sja1105pqrs spi0.0: 1 of 1 devices probed, final initialization
[    9.631917] sja1105pqrs spi0.0: 1 switch initialized successfully!
[    9.640658] [Roy_test ]attach_phydev 1160
[    9.644861] [Roy_test ]find_phydev 1117 port=0
[    9.649424] [Roy_test ]get_dt_node_for_port 1085
[    9.654165] [Roy_test ]get_dt_node_for_port 1093
[    9.660499] [Roy_test ]get_dt_node_for_port 1099 name=port-0
[    9.666397] [Roy_test ]find_phydev 1122 port_name=/lpspi@5a020000/sja1105p@0/port-0
[    9.676369] [Roy_test ]find_phydev 1131 port_name=/lpspi@5a020000/sja1105p@0/port-0
[    9.684151] sja1105pqrs spi0.0 SJA1105P_p0* (uninitialized): Port 0 does not have a (valid) phandle to an ethernet phy
[    9.694871] [Roy_test ]attach_phydev 1163 phydev=0
[    9.699824] sja1105pqrs spi0.0 SJA1105P_p0* (uninitialized): No phydev found for SJA1105P_p0*
[    9.709813] sja1105pqrs spi0.0 SJA1105P_p0*: Change link status of [SJA1105P_p0*] to: up
[    9.718130] sja1105pqrs spi0.0 SJA1105P_p0*: registered netdevice: [SJA1105P_p0*]
[    9.719073] sja1105pqrs spi0.0 SJA1105P_p0*: Change link status of [SJA1105P_p0*] to: up
[    9.725723] [Roy_test ]attach_phydev 1160
[    9.737942] [Roy_test ]find_phydev 1117 port=1
[    9.737950] [Roy_test ]get_dt_node_for_port 1085
[    9.747210] [Roy_test ]get_dt_node_for_port 1093
[    9.751986] [Roy_test ]get_dt_node_for_port 1099 name=port-1
[    9.758585] [Roy_test ]find_phydev 1122 port_name=/lpspi@5a020000/sja1105p@0/port-1
[    9.770142] [Roy_test ]find_phydev 1131 port_name=/lpspi@5a020000/sja1105p@0/port-1
[    9.777911] [Roy_test ]find_phydev 1141 port_name=/ethernet@5b050000/mdio/ethernet-phy@0 phydev=f7f89000
[    9.787495] [Roy_test ]attach_phydev 1163 phydev=f7f89000
[    9.792994] [Roy_test ]attach_phydev 1167
[    9.869729] sja1105pqrs spi0.0 SJA1105P_p1 (uninitialized): connected phy [8] (state: [9], link [1]) to port [1], attached_dev [SJA1105P_p1]
[    9.882710] sja1105pqrs spi0.0 SJA1105P_p1: Change link status of [SJA1105P_p1] to: down
[    9.890994] sja1105pqrs spi0.0 SJA1105P_p1: registered netdevice: [SJA1105P_p1]
[    9.891871] sja1105pqrs spi0.0 SJA1105P_p1: Change link status of [SJA1105P_p1] to: down
[    9.898384] [Roy_test ]attach_phydev 1160
[    9.910537] [Roy_test ]find_phydev 1117 port=2
[    9.915083] [Roy_test ]get_dt_node_for_port 1085
[    9.919802] [Roy_test ]get_dt_node_for_port 1093
[    9.924515] [Roy_test ]get_dt_node_for_port 1099 name=port-2
[    9.930288] [Roy_test ]find_phydev 1122 port_name=/lpspi@5a020000/sja1105p@0/port-2
[    9.930405] [Roy_test ]find_phydev 1131 port_name=/lpspi@5a020000/sja1105p@0/port-2
[    9.945804] [Roy_test ]find_phydev 1141 port_name=/ethernet@5b050000/mdio/ethernet-phy@1 phydev=f7f89800
[    9.955379] [Roy_test ]attach_phydev 1163 phydev=f7f89800
[    9.960878] [Roy_test ]attach_phydev 1167
[   10.037430] sja1105pqrs spi0.0 SJA1105P_p2 (uninitialized): connected phy [9] (state: [9], link [1]) to port [2], attached_dev [SJA1105P_p2]
[   10.050789] sja1105pqrs spi0.0 SJA1105P_p2: Change link status of [SJA1105P_p2] to: down
[   10.059547] sja1105pqrs spi0.0 SJA1105P_p2: registered netdevice: [SJA1105P_p2]
[   10.067056] [Roy_test ]attach_phydev 1160
[   10.071168] [Roy_test ]find_phydev 1117 port=3
[   10.075722] [Roy_test ]get_dt_node_for_port 1085
[   10.080461] [Roy_test ]get_dt_node_for_port 1093
[   10.084854] sja1105pqrs spi0.0 SJA1105P_p2: Change link status of [SJA1105P_p2] to: down
[   10.085370] [Roy_test ]get_dt_node_for_port 1099 name=port-3
[   10.100685] [Roy_test ]find_phydev 1122 port_name=/lpspi@5a020000/sja1105p@0/port-3
[   10.108789] [Roy_test ]find_phydev 1131 port_name=/lpspi@5a020000/sja1105p@0/port-3
[   10.118633] switch cluster 0 cpu-freq governor to schedutil
[   10.120648] [Roy_test ]find_phydev 1141 port_name=/ethernet@5b050000/mdio/ethernet-phy@4 phydev=0
[   10.133294] [Roy_test ]attach_phydev 1163 phydev=0
[   10.138205] sja1105pqrs spi0.0 SJA1105P_p3 (uninitialized): No phydev found for SJA1105P_p3
[   10.140739] switch cluster 1 cpu-freq governor to schedutil
[   10.147088] sja1105pqrs spi0.0 SJA1105P_p3: Change link status of [SJA1105P_p3] to: down
[   10.160569] sja1105pqrs spi0.0 SJA1105P_p3: registered netdevice: [SJA1105P_p3]
[   10.161624] sja1105pqrs spi0.0 SJA1105P_p3: Change link status of [SJA1105P_p3] to: down
[   10.167961] [Roy_test ]attach_phydev 1160
[   10.180409] [Roy_test ]find_phydev 1117 port=4
[   10.184973] [Roy_test ]get_dt_node_for_port 1085
[   10.189907] [Roy_test ]get_dt_node_for_port 1093
[   10.194648] [Roy_test ]get_dt_node_for_port 1099 name=port-4
[   10.202154] [Roy_test ]find_phydev 1122 port_name=/lpspi@5a020000/sja1105p@0/port-4
[   10.213190] [Roy_test ]find_phydev 1131 port_name=/lpspi@5a020000/sja1105p@0/port-4
[   10.220956] [Roy_test ]find_phydev 1141 port_name=/ethernet@5b050000/mdio/ethernet-phy@3 phydev=0
[   10.230147] [Roy_test ]attach_phydev 1163 phydev=0
[   10.235241] sja1105pqrs spi0.0 SJA1105P_p4 (uninitialized): No phydev found for SJA1105P_p4
[   10.244265] sja1105pqrs spi0.0 SJA1105P_p4: Change link status of [SJA1105P_p4] to: down
[   10.252809] sja1105pqrs spi0.0 SJA1105P_p4: registered netdevice: [SJA1105P_p4]
[   10.253930] sja1105pqrs spi0.0 SJA1105P_p4: Change link status of [SJA1105P_p4] to: down
[   10.316302] RTW: module init start
[   10.319736] RTW: rtl8821cs v5.8.1.1_35313.20191016_COEX20191014-4141
[   10.326316] RTW: build time: Feb 13 2022 11:17:29
[   10.331053] RTW: rtl8821cs BT-Coex version = COEX20191014-4141
[   10.336990] RTW: rtw_inetaddr_notifier_register
[   10.341835] RTW: module init ret=0
[   10.582219] audit: type=1006 audit(1599721382.432:2): pid=4131 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[   26.277602] random: crng init done
[   26.281021] random: 7 urandom warning(s) missed due to ratelimiting
[   50.915469] audit: type=1006 audit(1599721422.764:3): pid=4570 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=2 res=1
[ 1365.123174] audit: type=1006 audit(1599722736.972:4): pid=16287 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=3 res=1
[ 1629.702652] audit: type=1006 audit(1599723001.552:5): pid=18646 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=4 res=1

 

0 Kudos
Reply
1 Reply

1,625 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @ruge,

I hope you are doing well
 
Please confirm that you have set the Uboot environment variable accordingly for your display.
i.e U-Boot > setenv displayinfo  'video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24' 
 
Thanks & Regards,
Dhruvit Vasavada
0 Kudos
Reply