i.mx8mp yocto build with icecc(icecream)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx8mp yocto build with icecc(icecream)

1,803 次查看
Ivan_Lee
Contributor I

Hello,

regarding the build imx-yocto project with icecc(icecream),


I configured the environment as below for building yocto with icecc.

[Compiler PC]
1. install icecc : apt install icecc
2. added the icecc path on user account : export PATH="/usr/lib/icecc/bin:$PATH"
3. run iceccd : iceccd -m 2 -vv -d


[Scheduler PC]
1. install icecc : apt install icecc
2. start icecc-scheduler : sudo service icecc-scheduler start
3. added the icecc path on user account : export PATH="/usr/lib/icecc/bin:$PATH"
3-1. run iceccd : iceccd -m 2 -vv -d
4. download i.mx8mp source code as below
    repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.71-2.2.0.xml
    repo sync -j`nproc`
    EULA=1 MACHINE=imx8mpevk DISTRO=fsl-imx-xwayland source imx-setup-release.sh -b build_fsl-imx-xwayland
4. added the icecc related env in local.conf
    INHERIT += "icecc"
    ICECC_PARALLEL_MAKE = "-j 32"
    PARALLEL_MAKE = "-j 32"
    ICECC_PATH = "/usr/bin/icecc"
5. run bitbake : bitbake core-image-minimal

but, there is an error as below.
----------------------------------------
ERROR: /home/ivan/work4/sources/poky/meta/recipes-graphics/xorg-proto/xorgproto_2021.5.bb: /usr/lib/icecc/bin/gcc is a symlink to /usr/bin/icecc in PATH and this prevents icecc from working
ERROR: /home/ivan/work4/sources/meta-freescale/recipes-devtools/utp-com/utp-com_git.bb: /usr/lib/icecc/bin/gcc is a symlink to /usr/bin/icecc in PATH and this prevents icecc from working
ERROR: /home/ivan/work4/sources/meta-openembedded/meta-oe/recipes-support/libtinyxml/libtinyxml_2.6.2.bb: /usr/lib/icecc/bin/gcc is a symlink to /usr/bin/icecc in PATH and this prevents icecc from working
ERROR: /home/ivan/work4/sources/meta-openembedded/meta-oe/recipes-support/poco/poco_1.11.2.bb: /usr/lib/icecc/bin/gcc is a symlink to /usr/bin/icecc in PATH and this prevents icecc from working
ERROR: /home/ivan/work4/sources/poky/meta/recipes-graphics/xorg-proto/xorgproto_2021.5.bb: /usr/lib/icecc/bin/g++ is a symlink to /usr/bin/icecc in PATH and this prevents icecc from working
ERROR: /home/ivan/work4/sources/meta-freescale/recipes-devtools/utp-com/utp-com_git.bb: /usr/lib/icecc/bin/g++ is a symlink to /usr/bin/icecc in PATH and this prevents icecc from working

----------------------------------------

I'm a beginner at building with icecc.
is there anyone who help me?

regards,
Ivan

 

0 项奖励
回复
1 回复

1,782 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @Ivan_Lee 

Can't help provide support the build with icecream.

From these errors, as my understanding, it seems telling improper toolchain configured. 

 

Best regards

Harvey

0 项奖励
回复