[i.mx8mn][ddr4][ab2] I want to boot using emmc on ab2 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[i.mx8mn][ddr4][ab2] I want to boot using emmc on ab2 board

2,899 次查看
bryan_hong
Senior Contributor I

Hello

I have success the booting with SD card on ab2 board.
But I failed to booting with eMMC on ab2 board.

Below is the command I use to flash emmc.

uuu -b emmc_all imx-boot-imx8mnddr4ab2-ab2.bin-flash_ddr4_evk fsl-image-af-littlekernel-imx8mnddr4ab2-20220110053440.rootfs.wic

I want to know what command and what image file to use to download emmc to make booting successful.

thanks
Bryan

0 项奖励
回复
5 回复数

2,890 次查看
joanxie
NXP TechSupport
NXP TechSupport

should be the same images as you flashed to your sd card, what error do you get when you boot the board? did you flash the same images to the sd card successfully?

0 项奖励
回复

2,883 次查看
bryan_hong
Senior Contributor I

Hello joanxie

On SD card, I use below commands.

$bzip2 -d fsl-image-af-littlekernel-imx8mnddr4ab2-20210810094239.rootfs.wic.bz2

$sudo dd if=fsl-image-af-littlekernel-imx8mnddr4ab2-20210810094239.rootfs.wic of=/dev/mmcblk0 bs=1M conv=fsync

 

and I have attached error log for emmc boot fail.

[ 2.542605] mmc0: new ultra high speed SDR104 SDIO card at address 0001  <-- stucked

 

thanks

Bryan

0 项奖励
回复

2,867 次查看
joanxie
NXP TechSupport
NXP TechSupport

the command you use is correct, how about using this command to flash images to SD card? does it work?

"uuu -b sd_all imx-boot-imx8mnddr4ab2-ab2.bin-flash_ddr4_evk fsl-image-af-littlekernel-imx8mnddr4ab2-20220110053440.rootfs.wic"

0 项奖励
回复

2,853 次查看
bryan_hong
Senior Contributor I

Hello joanxie

===
uuu -b sd_all imx-boot-imx8mnddr4ab2-ab2.bin-flash_ddr4_evk fsl-image-af-littlekernel-imx8mnddr4ab2-20220110053440.rootfs.wic
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.139-0-g1a8f760

Success 1 Failure 0


1:13 6/ 6 [Done ] FB: done
===

and then The boot with sdcard was success. 

thanks
Bryan

 

0 项奖励
回复

2,826 次查看
joanxie
NXP TechSupport
NXP TechSupport

this should be your emmc issue, you need to check that, the images are fine

 

0 项奖励
回复