i.mx8m plus support lpddr4 and lpddr4x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.mx8m plus support lpddr4 and lpddr4x

跳至解决方案
5,915 次查看
zc_tee
Contributor III

Dear all,

May i know does i.mx8M Plus support both LPDDR4 and LPDDR4x RAM?

Thank you.

Regards,

Tee

0 项奖励
回复
1 解答
5,906 次查看
Yuri
NXP Employee
NXP Employee

@zc_tee 
Hello,

   I've sent You some comments directly.

Regards,
Yuri.

在原帖中查看解决方案

11 回复数
5,624 次查看
040869
Contributor I

Could I also get your comment? Interesting usage LPDDR4X >32Gb on own project.

Thanks!

0 项奖励
回复
5,805 次查看
richard_hu
Senior Contributor I

@Yuri 

Could I also get your comment?

We are considering to use LPDDR4X as well.

0 项奖励
回复
5,794 次查看
Yuri
NXP Employee
NXP Employee

@richard_hu 
  Done!

0 项奖励
回复
5,907 次查看
Yuri
NXP Employee
NXP Employee

@zc_tee 
Hello,

   I've sent You some comments directly.

Regards,
Yuri.

4,351 次查看
amigen-jason
Contributor IV

Yuri,

I'd like the comments as well.  We would like to use an LPDDR4X with the i.MX 8MPlus purely for power savings (not increased bandwidth), if possible. 

 

We currently run LPDDR4 at 800 MHz as our systems do not have intensive memory bandwidth requirements, but do have extreme low power requirements (on battery).

0 项奖励
回复
5,003 次查看
aviad_h
Senior Contributor I

@Yuri 

Can you please share comments 

0 项奖励
回复
5,532 次查看
torus1000
Contributor V

@Yuri 

Could I also get your comment? Thanks!

0 项奖励
回复
5,528 次查看
Yuri
NXP Employee
NXP Employee

@torus1000 
Hello,

   The 8M Plus does not support LPDDR4x.

Regards,
Yuri.

0 项奖励
回复
5,748 次查看
anhui527
Contributor III

Could I also get your comment? thanks.

0 项奖励
回复
5,741 次查看
Yuri
NXP Employee
NXP Employee

@anhui527 
Hello,

  I've sent You comments in Case Number 00328551.

Regards,
Yuri.

0 项奖励
回复
5,902 次查看
zc_tee
Contributor III

Thank you! got your comment already.

Regards,

Tee

0 项奖励
回复