i.mx8m plus in yocto 5.4.24_2.1.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8m plus in yocto 5.4.24_2.1.0

Jump to solution
1,054 Views
zc_tee
Contributor III

Dear all,

May i know does yocto 5.4.24_2.1.0 supports i.mx8m plus platform?

I done the repo download for yocto 5.4.24_2.1.0, and when i try to build for i.mx8m plus evk board, i realise the machine selection available for imx8 under meta-freescale/conf/machine/ is only imx8mmevk, imx8mqevk, imx8qmmek and imx8qxpmek.

How can i build for i.mx8m plus?

Thank you.

Regards,

Tee

0 Kudos
Reply
1 Solution
1,041 Views
Yuri
NXP Employee
NXP Employee

@zc_tee 

Hello,

   According to i.MX Yocto Project User's Guide (Rev. L5.4.24)
" imx8mpevk" machine configuration can be used.

 

Regards,
Yuri.

View solution in original post

0 Kudos
Reply
2 Replies
1,042 Views
Yuri
NXP Employee
NXP Employee

@zc_tee 

Hello,

   According to i.MX Yocto Project User's Guide (Rev. L5.4.24)
" imx8mpevk" machine configuration can be used.

 

Regards,
Yuri.

0 Kudos
Reply
1,016 Views
zc_tee
Contributor III

Thank you! it can compile now.

Regards
Tee

0 Kudos
Reply