i.mx8m nano boot from qspi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx8m nano boot from qspi

10,883件の閲覧回数
klaus_dannecker
Contributor I

my evalboard is 8MNANOD4-EVK
I want to boot via the QSPI interface.
How do i have to configure the U-boot for this?
(https://gitlab.denx.de/u-boot/u-boot)

Background:
i would like to make my own board based on this evalboard, but with only the QSPI interface for booting.

ラベル(1)
0 件の賞賛
返信
15 返答(返信)

10,352件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Klaus

one can check uboot sources, in particular : #ifdef CONFIG_FSL_FSPI

imx8mn_evk.c\imx8mn_evk\freescale\board - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

10,352件の閲覧回数
klaus_dannecker
Contributor I

Hi Igor

until now i have always cloned the repository of https://gitlab.denx.de/u-boot/u-boot I thought this is the original one.

If i now clone the branch imx_4.14.98_8qxpc0_er, am i always up to date?
In the future i want to work with the evalbord imx8m nano with LPDDR. This should be released Q1. The design files are already on the homepage.

Best regards

Klaus

0 件の賞賛
返信

10,352件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Klaus

main line uboot is not supported by nxp, issue may be posted on

U-Boot Info Page 

Supported uboot from source.codeaurora.org/external/imx repository : uboot-imx - i.MX U-Boot 

as described in official nxp linux documentation Linux 4.19.35_1.1.0 Documentation

i.MX Software and Development Tools | NXP 

Best regards
igor

0 件の賞賛
返信

10,352件の閲覧回数
klaus_dannecker
Contributor I

Hi igor,

is it correct that for booting over qspi I only need to write the following lines in the file imx8mn_ddr4_evk_defconfig must change?

CONFIG_SYS_EXTRA_OPTIONS="IMX_CONFIG=arch/arm/mach-imx/spl_sd.cfg,SPL_TEXT_BASE=0x912000"
to
CONFIG_SYS_EXTRA_OPTIONS="IMX_CONFIG=arch/arm/mach-imx/spl_qspi.cfg,SPL_TEXT_BASE=0x912000"
do I need a different SPL_TEXT_BASE address?

add
CONFIG_SPL_NOR_SUPPORT=y

in the original file are CONFIG_ENV_IS_IN_MMC=y and CONFIG_ENV_IS_IN_SPI_FLASH=y

shouldn't there be only one specification? The ENV cannot be in both positions!

in the i.MX_Porting_Guide.pdf:

f. For i.MX 8, use the imx-mkimage tool to combine the U-Boot binary with Arm
Trusted Firmware (ATF) and SCFW to produce the final flash.bin boot image
and burn to the SD card. See the imx-mkimage tool for details.

Where can I get the right imx-mkimage tool, ATF and SCFW FW?

Is there no tutorial to create the final flash.bin boot image?

Best regards

Klaus

0 件の賞賛
返信

10,352件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

For the 8M-Mini platform please also read here:  https://community.nxp.com/docs/DOC-343777 

Regards,

Bernhard.

0 件の賞賛
返信

10,352件の閲覧回数
klaus_dannecker
Contributor I

Hi Bernhard,

i don't use yocto! i do not need linux, i work with vxWorks!

I would like to make the uboot standalone with a crosscompiler.

Regards,

Klaus

0 件の賞賛
返信

10,352件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Klaus

nxp does not support vxWorks, issue may be posted

on Wind River Customer Support 

Supported building using yocto, details can be found in

Yocto Guide included in Linux 4.19.35_1.1.0 Documentation

Best regards
igor

0 件の賞賛
返信

10,352件の閲覧回数
klaus_dannecker
Contributor I

Hi igor,

i only want to make the u-boot with a crosscompiler!

Command:

make imx8mn_ddr4_evk_defconfig

make flash.bin

and now i become a error! (see last message)

nxp support this one, right?

Best regards
Klaus

now i have found the error!

There is a bug in /tools/imx8mimage.c

The variable using_fit is only set when the comand SIGNED_HDMI is in the spl/u-boot-spl.cfgout File.

But the imx8mn don't use this comand!

change the parse_cfg_fld() to:

static void parse_cfg_fld(int32_t *cmd, char *token,
              char *name, int lineno, int fld)
{
    switch (fld) {
    case CFG_COMMAND:
        *cmd = get_table_entry_id(imx8mimage_cmds,
                      "imx8mimage commands", token);
        if (*cmd < 0) {
            fprintf(stderr, "Error: %s[%d] - Invalid command" "(%s)\n",
                name, lineno, token);
            exit(EXIT_FAILURE);
        }
        switch (*cmd) {
        case CMD_FIT:
            using_fit = 1;
            break;
        }
        break;
    case CFG_REG_SIZE:
        parse_cfg_cmd(*cmd, token, name, lineno);
        break;

...

...

and remove in parse_cfg_cmd()

    case CMD_SIGNED_HDMI:
        signed_hdmi = token;
/*    case CMD_FIT:
        using_fit = 1;*/
        break;
    case CMD_DDR_FW:
        /* Do nothing */
        break;
    }

Best regards
Klaus

0 件の賞賛
返信

10,352件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Klaus

I sent additional  build document via mail.

Best regards
igor

0 件の賞賛
返信

10,352件の閲覧回数
klaus_dannecker
Contributor I

Hi igor,

the Document  is ok.

but it's from an obsolete stand.
there you had to create the file to flash in two separate steps.
1. generate uboot
2. mkimage

in the new branch can you generate the file to flash in one step.

1. generate file with

    make flash.bin

-> the makefile generate uboot and mkimage internal.

for the  imx8qm Board it works fine!

It use the SIGNED_HDMI File

but the imx8m nano don't use it! so the internal mkimage generate a error!

Regards

Klaus

ps: see last messages!

0 件の賞賛
返信

10,352件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Klaus

 

please check document chapter for i.MX8MQ (Nano is similar to MQ) not i.MX8QM.

 

Best regards
igor

0 件の賞賛
返信

10,352件の閲覧回数
klaus_dannecker
Contributor I

Hi igor

now I have done everything as described in the document, and try to build a flash.bin

1. Build u-boot

    unset LDFLAGS
    make -j8 imx8mn_ddr4_evk_defconfig
    make -j8 

output:

...

  COPY    spl/u-boot-spl.bin
make[1]: Nothing to be done for 'SPL'.
===================== WARNING ======================
This board does not use CONFIG_DM_VIDEO Please update
the board to use CONFIG_DM_VIDEO before the v2019.07 release.
Failure to update by the deadline may result in board removal.
See doc/driver-model/MIGRATION.txt for more info.
====================================================
  CFGCHK  u-boot.cfg

i ignor this Warning.

2. Coppy following Files to imx-mkimage/iMX8M/:

  bl31.bin

  ddr4_dmem_1d.bin

  ddr4_dmem_2d.bin

  ddr4_imem_1d.bin

  ddr4_imem_2d.bin

  u-boot.bin

  spl/u-boot-spl.bin

  u-boot-nodtb.bin

  arch/arm/dts/fsl-imx8mn-ddr4-evk.dtb

according to the document you should copy lpddr4_pmu_train_1d_dmem.bin ...

This board have no LPDDR4! it has DDR4, so i copy  ddr4_dmem_1d.bin ...

3 generate flash.bin

  make clean
  make SOC=iMX8MN flash_spl_uboot   ( in dokument make SOC=iMX8M flash_spl_uboot)

output:

...
 PLAT=imx8mn HDMI=no
 Compiling mkimage_imx8
 gcc  -O2 -pipe -g -feliminate-unused-debug-types  mkimage_imx8.c -o mkimage_imx8 -lz
 make[1]: *** No rule to make target 'lpddr4_pmu_train_1d_imem.bin', needed by 'u-boot-spl-ddr.bin'.  Stop.
 make: *** [Makefile:20: flash_spl_uboot] Error 2

why is lpddr4 required here?

ok, i copy the lpdd4-Files to imx-mkimage/iMX8M/ an generate once again.

output:

  PLAT=imx8mn HDMI=no
  Compiling mkimage_imx8
  gcc  -O2 -pipe -g -feliminate-unused-debug-types  mkimage_imx8.c -o mkimage_imx8 -lz
  make[1]: *** No rule to make target 'fsl-imx8mn-evk.dtb', needed by 'u-boot.itb'.  Stop.
  make: *** [Makefile:20: flash_spl_uboot] Error 2

i have use following imx-mkimage:

git clone https://source.codeaurora.org/external/imx/imx-mkimage -b imx_4.14.98_2.3.0

Well, it doesn't seem quite that simple!

What am I doing wrong?

Best regards
Klaus

ps:

when i make step1 with branch imx_4.14.98_8qxpc0_er become i no warning!

but the error on step3 is the same!

what branch of u-boot and imx-mkimage is the rigth?

0 件の賞賛
返信

10,342件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Klaus

suggest to build using sect.5.3 Building an image attached Yocto Guide.

Best regards
igor

0 件の賞賛
返信

10,342件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Klaus

for i.MX8M (same for Mini,Nano) one can look at

https://developer.solid-run.com/knowledge-base/i-mx8m-atf-u-boot-and-linux-kernel/ 

https://boundarydevices.com/yocto-release-for-i-mx-8mm/ 

QSPI boot can be tested on i.MX8M Mini EVK using Demo Images on

i.MX Software and Development Tools | NXP 

SCFW is not used for i.MX8M, it is used for i.MX8QM, QXP.

Best regards
igor

0 件の賞賛
返信

10,342件の閲覧回数
klaus_dannecker
Contributor I

Hi Igor,

now i checkout the branch imx_v2019.04_4.19.35_1.1.0

I hope this is right.

i still get the following error:

...

arch/arm/dts/fsl-imx8mn-ddr4-evk.dtb > u-boot.its
bl31.bin size:
37209
u-boot-nodtb.bin size:
706552
arch/arm/dts/fsl-imx8mn-ddr4-evk.dtb size:
25791
  MKIMAGE u-boot.itb
u-boot.its:7.11-14.5: Warning (unit_address_vs_reg): /images/uboot@1: node has a unit name, but no reg property
u-boot.its:15.9-23.5: Warning (unit_address_vs_reg): /images/atf@1: node has a unit name, but no reg property
u-boot.its:24.9-29.5: Warning (unit_address_vs_reg): /images/fdt@1: node has a unit name, but no reg property
u-boot.its:34.12-39.5: Warning (unit_address_vs_reg): /configurations/config@1: node has a unit name, but no reg property
./tools/imx8m_image.sh spl/u-boot-spl.cfgout 1
  MKIMAGE flash.bin

make[1]: *** [arch/arm/mach-imx/Makefile:210: flash.bin] Error 1
make[1]: *** Deleting file 'flash.bin'
make: *** [Makefile:1273: flash.bin] Error 2

 

Best regards

Klaus


					
				
			
			
				
			
			
				
			
			
			
			
			
			
		
0 件の賞賛
返信