i.mx8m mini evk i2c3,mipi-csi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8m mini evk i2c3,mipi-csi

616 Views
grif
Contributor I
I am trying to control i2c3 and mipi-csi on M4 side with i.mx8m mini evk. On the A53 side, linux (L4.19.35._1.1.0) is running. Accessing the i2c3 and mipi-csi registers on the M4 side stops. I don't know how to deal with it. (Device tree file?) Please professor.
0 Kudos
1 Reply

546 Views
igorpadykov
NXP Employee
NXP Employee

Hi Osamu

i2c3 is already supported in SDK_EVK-MIMX8M Mini available on Welcome | MCUXpresso SDK Builder 

in folder ..driver_examples/i2c

So on below fsl-imx8mm-evk-m4.dts  i2c3 is disabled

fsl-imx8mm-evk-m4.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

For mipi-csi it is necessary to perform similar steps: disable in linux dts and add driver to SDK.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos