i.mx8MM ddr4 board nand flash size change ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx8MM ddr4 board nand flash size change ?

ソリューションへジャンプ
3,510件の閲覧回数
weikeng-jimmy
Contributor III

Hi Sir,

            I write NAND boot image into NAND flash (64G) and switch the mode to NAND boot , the Imx8mm EVK can boot up successful.  I will change NAND flash size from 64G (MT29F64G08CBABBWP) to 8G (MT29F8G08ABACA) , it's not boot up.  I try to switch the "pages in block to 01-64" , but it's still not boot up .

Did I lose any steps or moves?

未命名.png

U-Boot SPL 2018.03-00012-g87a19df-dirty (Oct 02 2019 - 17:53:43 +0800)

.......

Trying to boot from NAND

 

 

U-Boot 2018.03-00012-g87a19df-dirty (Oct 02 2019 - 17:53:43 +0800)

 

CPU:   Freescale i.MX8MMQ rev1.0 at 1200MHz

CPU:   Commercial temperature grade (0C to 95C) at 37C

Reset cause: POR

Model: FSL i.MX8MM DDR4 EVK board

DRAM:  2 GiB

TCPC:  Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]

Power supply on USB2

TCPC:  Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]

NAND:  8192 MiB

MMC:   FSL_SDHC: 0

Loading Environment from NAND... *** Warning - bad CRC, using default environment

ラベル(3)
0 件の賞賛
返信
1 解決策
3,368件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JIMMY

patch was sent via mail.

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,369件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JIMMY

patch was sent via mail.

Best regards
igor

0 件の賞賛
返信
2,875件の閲覧回数
adam_szastok
Contributor I

Hi

Could You send me this patch via email

Best regards

Adam

0 件の賞賛
返信
3,368件の閲覧回数
weikeng-jimmy
Contributor III

Yes, Thanks~

0 件の賞賛
返信
3,368件の閲覧回数
weikeng-jimmy
Contributor III

The issue solved ~ Thanks!

0 件の賞賛
返信
3,097件の閲覧回数
fernando_lopes
Contributor II

Hi @weikeng-jimmy!

I'm having the same issue you had with your NAND flash. I'm also using an 8Gbit NAND and I couldn't boot the i.MX8MM using it yet.

What is the patch you had to use to fix the problem? Could you help me with that? 

Thanks!

0 件の賞賛
返信